Part Number: TPS7A49 Hello LDO Team,
I'm an applications engineer from DLP team developing an EVM featuring your device, TPS7A49. Taking 12V input, generating 10V and 5V rails. Please let me know if you have any suggestions to improve the schematic…
Part Number: TPS7A49
Dear Team,
We purchased the TPS7A4901DRBT from DigiKey. However, the marking on the received component appears to be different from what we expected, and we are unable to identify the part number based on the information provided…
Part Number: TPS7A49 Other Parts Discussed in Thread: UCC28950 Hi,
The above LDO was used in bootstrap configuration in half bridge circuit. That Bootstrap LDO was failed which resulted into MOSFET failure. After replacing LDO and MOSFET, converter…
Part Number: TPS7A49 Tool/software: Dear team,
I am currently reviewing the TPS7A49 datasheet and have a question regarding the calculation of R2 in the adjustable output configuration.
In equation (2) on page 14, it is written as:
VFB(nom)/R2>5μA…
Other Parts Discussed in Thread: TPS7A19 Tool/software: We are looking for an LDO with VIN = +24V and Vout = 3.3V or 5V, I_out = 150mA, T_JA < 50 C/W and optionally with soft start feature. We liked TPS7A19 for its size and heat dissipation but it is…
Part Number: TPS7A49 Tool/software: Hi Team
Please help to review the design below and provide your feedback.
Input Voltage: 6.5V
Output Voltage: 1.8V
Load current: 92mA
Thanks in advance,
Regards
Haritha
Part Number: TPS7A49 Tool/software: We are using this LDO (15V to 6.5V) in the bootstrap circuit to power the high-side FET in a PSFB ZVT converter. During module switching, we have observed that the LDO intermittently turns off. Please refer to the attached…
Part Number: TPS7A49 Tool/software: hello,
We are using the TPS7A49 in the below circuit.
When OUT=8V, we short R48, connected to R49 and the FB pin, so TPS7A49 OUT changes from 8V to 15V (R48 shorted via transistor for OUT=15V and connected for…
Part Number: TPS7A49 Other Parts Discussed in Thread: LMX1214 , TPS7A94 Tool/software: Hi Team,
As per the above image we are feeding 12V from external and generating 6.5V.
from 6.5V old circuit has P/N: TPS7A4901 and evaluation board has (P/N…
Part Number: TPS7A49 Other Parts Discussed in Thread: TPS61288
Tool/software:
Hello. This is Kwonjoon Lee from South Korea.
I would like to ask about a discharging operation of the TPS7A4901.
(Detailed Situation)
1. The VIN of my TPS7A4901…