Part Number: TPS7A49 Hello im currently doing a project for my university designing a circuit involving the tps7A49. However i would like to test the circuit with a breadboard before finalizing it on a pcb.
So my question would be: Are there any sockets…
Part Number: TPS7A49 Looking through the datasheet for the TPS7A49 and looking at the typical application example. Specifically page 17. Equation 5 calculation of R1. The calculations comes out to 1.265K. However, the next line says to select R1 at a…
Part Number: TPS7A49 Other Parts Discussed in Thread: TPS717 , TPS7A39 , Hi team,
Is there a graph of PSRR vs (Vin-Vout)? I want PSRR data other than Vin = 6.2V, Vout = 5V in the datasheet.
Because it is necessary to determine PSRR performance and…
Part Number: TPS7A49 Hello,
I'm a reliability engineer currently conducting a trade study involving this part. Is there a factor of 10 estimate for the number of transistors in this device? Similarly, are these BJT type or some other kind?
Thank…
Part Number: TPS7A49 Hi,
Input is 16.5V from the output of a switcher which has good load regulation. For some reason I'm getting a 400mV drop out of this LDO from 15.2V down to 14.8V when I load the output with 100mA. I can't see anything obvious.…
Part Number: TPS7A49 Hi
We use TPS7A4901DGNR in 5.6V to 5.0V voltage regulator, typical output current is about 75-80mA.
The PCB is in production from 2014. No an issue till November, 2019.
Starting from the end of November we experienced reduced…
Part Number: TPS7A49 Other Parts Discussed in Thread: TPS7A4001 Tool/software: WEBENCH® Design Tools Hello
i have some problem with TPS7A49 ic simulation
i tried some different values of Vout and always i get big error voltage
for example, with…
Part Number: TPS7A49 Other Parts Discussed in Thread: ASH Immediate request please:
PN TPS7A4901DGNR has a lead finish of NIPDAU|NIPDAUAG - how it is determined which finish we will receive? We want to only get the NiPdAu finish as the NiPdAuAg finish…
Part Number: TPS7A49 We are designing a PCB which would be enclosed in a cylindrical plastic cabinet and would be filled with a potting material having thermal conductivity of 0.45 W/m K.
We are using TPS7A49 LDO (VSON-8 Package) to convert 15V DC…
Part Number: TPS7A49
could you share the resistance from EN to IC GND?
does it recommend that customer connect a 10k resister between en and Vin?
what if voltage of EN to Vin lager than the maximum value in the table?