Part Number: TPS7A52-Q1 Hi all,
I want to simulate this for noise, however only transient model is available. Is there an AC model available for noise analysis?
Thanks,
Kay
Part Number: TPS7A52-Q1 Other Parts Discussed in Thread: TIDA-01022 Hello! At the moment, I am developing a printed circuit board that is very remotely similar to TIDA-01022. There are many power lines on the board that need to be separated by LC-filters…
Part Number: TPS7A52-Q1 Other Parts Discussed in Thread: TPS7A52 I found a couple of bugs with the unencrypted SPICE model this device.
1. The text file, line 34, is missing a comment character. This prevents TINA from importing the model- please fix this…
Part Number: TPS7A52-Q1 Hello TI team
When do you release new version of Data Sheet?
I prefer to have the data sheet below speck is referred.
VEN (Enabel Voltage Range)
Min:0V
Max:6.5V
Thank you,
Tanaka,
Part Number: TPS7A52-Q1 Hi Team,
My customer are request the IBIS or IBIS AMI model for some parts, can you provide its ?
Part number: TPS7A5201WQRTKRQ1
Thanks & regards,
Kai
Part Number: TPS7A52-Q1 Dear,
I'm unable to find the initial tolerance of the feedback voltage in the datasheet of the component, there is only a typical value.
Could someone give me the min and max value?
Regards
Matthieu Baque
Part Number: TPS7A52-Q1 Hi team,
Could you check what will happen if enable pin floating?
If there is any pull up inside enable pin so the Vout will still ramp up?
Regards,
Allen
Part Number: TPS7A52-Q1 Hello,
I saw on the datasheet of the TPS7A52-Q1 that the deviation of the accuracy of the output voltage (without bias and between -40°C and +125°C) is -1% and +1%.
I would like to know if it includes ageing.
Thanks,
Ne…
Part Number: TPS7A52-Q1 Hi,
using the TPS7A52-Q1 to have a stable 1,95V voltage at the Output. Supply it with stable 5V from another LDO.
On my first PCB where I designed it on I see that it is quite often showing the correct 1,95V (without load). Sometimes…