Part Number: TPS7A53 Hi Sir,
after our review, we do not see any issue, do you have any suggestion or recommend change for this circuit? thanks for you support and learn from you.
Part Number: TPS7A53 Tool/software: Hi everyone,
I’m Simon, currently working on a circuit design using TI’s TPS7A53 LDO regulator. My application requires a 0.8V output, which appears to be the minimum voltage supported by this device according to…
Part Number: TPS7A53 Tool/software:
Hello, i m designing a schematic using the TPS7A5301RPSR to power up an LTE module. he LDO output target is a 3.7V, 3A and 5V input. Is the schematic is acceptable in the picture below? Also is it recommended to use…
Part Number: TPS7A53-Q1 Other Parts Discussed in Thread: TPS7A85 , Hello team,
Load regulation at Vout = 5V is different between TPS7A5301QRGRRQ1 and TPS7A8500ARGRR.
Can you clarify which one is correct?
Best Regards,
Austin
Part Number: TPS7A53 Tool/software: Team,
Can you please clarify the following on the TPS7A5301 LDO’s?
The max V spec for the EN pin is 6.5V
The max V spec for the Vin pin is 6.5V
The max V spec for the Vbias pin is 6.5V
Are the max voltages…
Part Number: TPS7A53 Hello,
for our design I'd like to use the TPS7A53 as a low-noise reference power sources, powering analog devices such as ADCs, HF-module and MCU all at once.
( https://www.ti.com/lit/ds/symlink/tps7a53.pdf?ts=1680723465539&ref_url…
Part Number: TPS7A53 Other Parts Discussed in Thread: TPS7A57 , TPS7A84 , Hi Team,
Is there comparison between TPS7A53 and TPS7A57 and TPS7A84? Thanks.
BRs
Given
Part Number: TPS7A53 Hi,
I am using TI LDO - TPS7A5301RPSR for my design.
Can you please advise if the component can be damaged in case I set it as Disabled (J313) but I will connect an External Power (J310) to the LDO power rail?
V_IN = 1.5V (stay…
Part Number: TPS7A53-Q1 Hi,
We are using TPS7A5301QRGRRQ1 LDO in our design for 3.3V-1.8V conversion ,3.3V-1V conversion and 5V-1.2V conversion.
Kindly review the design and share the comments.
3.3V-1.8V conversion
3.3V-1V conversion
5V…
Part Number: TPS7A53 Hello TI,
1> In case of LDO part TPS7A53 (3A or 4A part), to what voltage Power Good (PG) resistor should be pulled up to? What is recommended? Pull it up to Vin or Vout?
2> When we are driving EN signal of second TPS7A53 from…