Part Number: IWR1843 Other Parts Discussed in Thread: LP87702 , TPS7A53 Tool/software: Hello, I'm Mark.Kim
Recently, I'm working on a RADAR Board design using IWR1843.
Power line on IWR1843ISK EVB Board: LM53635 - LP87702 - TPS7A53
It uses DC 5V…
Part Number: TPS7A84A Other Parts Discussed in Thread: TPS7A53-Q1 , , TPS7A84 Tool/software: Hi,
The graphs of PSRR, noise characteristics and transient response on the data sheet of the following products are the same. Could you tell me the reason…
Part Number: TPS56528 Other Parts Discussed in Thread: TPS7A53 , I just noticed that unlike most other parts with internal aux regulator, there's no explicit prohibition not to load the VREG5. There's even I O_VREG5 specified. Is it allowed to load it…
Part Number: LP3856 Other Parts Discussed in Thread: TPS7A53 , TPS7A54 Hi,
Good Day.
If LP3856ES-2.5/NOPB (2.5V/3A) recommended for Voltage rail to an FPGA device?
Please advise. Thank you very much.
Best Regards,
Ray Vincent
Part Number: TPS7A92 Other Parts Discussed in Thread: TPS7A94 , TPS7A96 , TPS7A53 Hi,
We are using TPS7A92 in our project.
But during bringup of the board, we came to know we need higher current for the IC which is powered by TPS7A92.
So, please…
Part Number: TPS7A74 Other Parts Discussed in Thread: TPS7A57 , TPS7A54 , TPS7A53 Dear Sirs,
May I use 2 LDOs in parallel to get a double output current?
My customer wants to use 2pcs TPS7A7401 to do such design.
Please help to advise.
Thanks…
Part Number: TPS755 Other Parts Discussed in Thread: TPS7A53 ,
Hi team,
The customer would like to use TPS75533KTT for high current applications:
The output is 3.3V at an input voltage of 5V, with a voltage drop of 1.7V. Based on the maximum current…
Part Number: TPS7A53A-Q1 Other Parts Discussed in Thread: TPS7A53-Q1 , Dear team,
I have a question about Vbias voltage. TPS7A53-Q1 (non-A product) accepts the Vbias = floating and no use. But I think that TPS7A53A-Q1 does not accept Vbias = open and…
Other Parts Discussed in Thread: LM5155 , TPS7A57 , TPS7A52 , TPS7A53 , LM317 , TPS7A47 I am working on the design of single input multi output dc-dc converter with following specifications.
Input 28 V dc (16 V - 48V)
Outputs are 5V, 8A ; 5V…
Hi Ann,
Most positive LDO's only have the ability to source current. They do not normally have the ability to sink current. If Vout happens to be higher than the intended regulation voltage, the LDO simply stops sourcing current to the load.
In terms…