Part Number: TPS7A53B Hi,
In Table 6-2 of the DS, it shows:
It shows even Vbias is out of UVLO the chip will be off under any Vin and EN, right?
Thanks.
Part Number: TPS7A53B Other Parts Discussed in Thread: ADC12D1000 Hello, I am using this TPS7A53B to supply the ADC12D1000. The current derating used is 70%, which means 2.1A. 2.1A max for the ADC + 20% of margin is above the 2.1A. Also, the thermal resistance…
Part Number: TPS7A53B Tool/software: What is the state of PG if the device is unpowered? Floating so that external pullup will declare power good?
Or is it held low via clamp diode?
Part Number: TPS7A53B Tool/software: Looking to select a Schottky diode for reverse current protection. In the data sheet, it suggests the max rating of Vout > Vin + 0.3V. If interpreting this correctly, I would need a Schottky diode with a forward voltage…
Part Number: TPS7N49 Other Parts Discussed in Thread: ADC12D1000 , TPS7A53B , TPS7A53 Hello, I am consideraring to use TPS7N49 to supply the ADC12D1000. I want to filter all noise as possible tfrom the power supply. the DCDC used has fs = 1.5MHz. Is TPS7N49…
Part Number: ADC12D1000 Other Parts Discussed in Thread: TPS7A53B , TPS7N49 , TPS7A53 Hello, I have a question regarding the current consumption. According to datasheet supply current is 2.105A for ADC12D1000. What is the margin that I have to use for…
Part Number: TPS7A84 Other Parts Discussed in Thread: TPS7A53B , Tool/software: Hi team,
My customer is looking for an alternatives to replace with TPS7A8400.
And the LDO should have the similar Vin range, and 3A output current capability.
But the…
Other Parts Discussed in Thread: LMQ64480-Q1 , LMR14050 , TPS7A53B Hi Expert,
Could you recommend a buck solution with auto spec? thanks!
Input:12V(typ) 36V(max)
Output:0.8V/ 0.9V
Current: 3A
Far
Part Number: TPS7A94 Other Parts Discussed in Thread: TPS7A14 , TPS7A53B Hi, I have a board I'm working on that requires the following power rails:
19V @ 2A
5V @ 3A
3V3 @ 1A
1V05 @ 1A
I'm trying to figure out whether I should be using 4…