Part Number: TPS7A57 Hello, Referring to the block diagram in the data manual, is the 200uA current source powered by VBIAS or VIN? The 200uA current source and the charging pump are connected together. Can I understand if this current source is connected…
Part Number: TPS7A57 Tool/software: Hello,
In the customer's project, TPS7A57 is used with an output voltage of 3.3V. May I know the minimum voltage for input and Vbias, how to handle the CP.EN pin, and how to apply it? Thanks!
Part Number: TPS7A57 Other Parts Discussed in Thread: TINA-TI
Tool/software:
I downloaded the Spice model and trying to create a Macro Model with the CIR file it says it's empty. It's not empty but it doesn't look like anything Tina Ti will import…
Part Number: TPS7A57 Tool/software: Hello, good afternoon. How to connect a TPS7A57 as a current source for a very specific application. My load has low resistance (between 0.5 ohms and 1.5 ohms) and I want to apply a direct current of 3 amps to it. If…
Part Number: TPS7A57 Hello Team
I have a question regarding the determination of the BIAS voltage for TPS7A57.
In the datasheet, on page 56 (Note section), it states that when the internal charge pump is disabled, the BIAS voltage must satisfy the…
Part Number: TPS7A57 Dear Team, Happy new year. I want to know about is there any alternate LDO part available for the following conditions. I have 2 major Condition.
1, It has to be AEC Qualified. 2, It has to be part with -55°C to 125°C Temp support…
Part Number: TPS7A57 I'm studying the part with ChatGPT and it doesn't like any case where I have BIAS at 3.3V. With no charge pump on it says it needs to be 5V. ChatGPT even makes it seems like TI offers no assurance the part works without the charge…
Part Number: TPS7A57 Tool/software: Hello,
My customer requested a review from TI for their TPS7A5701RTER design below.
Please review the circuit design to see if there are any problems.
TPS7A5701RTET SCH.PDF
Thank you.
JH
Part Number: TPS7A57 Hello,
Instead of a set resistor attached to REF to set the voltage on the error amplifier can this be a voltage reference instead? It believe it would need to be able to SINK IREF, but is there any other issues with providing a…
Part Number: TPS7A57 Other Parts Discussed in Thread: TL431
Tool/software:
Good morning,
I have a query on TPS7A57 as follows.
The transient response of the LDO is shown in datasheet image 6.33-6.36.
I notice that there is no ringing in the…