Part Number: TPS7A63-Q1 Hello Team,
The recommended value of Cin in the data sheet is stated as follows.
・Cin = 10~22uF (300mAmax)
Is it necessary to use the same Cin even when Iout=100mA(max)? Currently, 4.7uF x 2 is used. Is there a problem?
Best regards…
Part Number: TPS7A63-Q1 Dear TI:
i want to know what's the relationship between output capacitance and transient response? input volt: 12V , Output volt: 5v and the load Current total only 130mA . output capacitance total about 10uf+0.1uf*7 when…
Part Number: TPS7A63-Q1 Dear TI:
TPS7A6350Q1 Input Volts vs Reset Table as fellows. Does different input volts can affect the reset Time or not? i can't find related files in datasheet. thanks a lot
for example: t_delay=300ms; when input volt=5V…
Part Number: TPS7A63-Q1 Hello Team,
The output accuracy specification is ±2%, what is the accuracy at 25℃? I want to know the temperature characteristic of output accuracy.
Best regards, Kato
Part Number: TPS7A63-Q1 Hello Team,
Please tell me the value of the internal pull-down resistor of the pin below.
- EN - nWD_EN
It is necessary to determine the value of the external pull-up resistor.
Best regards, Kato
Part Number: TPS7A63-Q1 Other Parts Discussed in Thread: TPS7B63-Q1 Team,
I'm FAE in TI Korea Automotive Team.
There is reset issue that LDO resets during low voltage input test down to 4V. Since TPS7A6350-Q1 resets when output voltage goes down to…
Part Number: TPS7A63-Q1 Other Parts Discussed in Thread: TPS7B63-Q1 Dear, All
Customers are considering circuits using TPS7A6350-Q1. They have 2 questions a. Power-on-reset delay time For Power-on-reset delay time, only Typ value is listed in the data sheet…
Part Number: TPS7A63-Q1 Hello Team,
When the nWD_EN pin is set to Disable->Enable(High->Low), how long is it from the falling edge to the completion of initialization?
Best regards, Kato
Part Number: TPS7A63-Q1 Dear TI engineer
My customer has question for TPS7A6350-Q1 enable pin level.
In D/S,
customer test result is
low level : about 1.35V, high level : about 1.7V
first of all, why is it so much better than the stated value?
is this…