Part Number: TPS7A66-Q1 Hello, Could you advise how long the enable needs to be pulsed low to trigger a reset of the LDO? Also, what is the delay between EN falling from 3.3V -> 0V and the LDO shutting off the output.
Thank you!
Part Number: TPS7A66-Q1 Hi team,
I would like to know PG operation.
When the power is good, PG output will be high impedance and PG pin is pull high to Vout. So PG pin will be high. When the power is not good(Vin=0), PG output will be low impedance and…
Part Number: TPS7A66-Q1 Hi Team,
I see the PG comments in datasheet.
Power good. This open-drain pin must connect to VOUT via an external resistor. VPG is logic level high when VOUT is above the power-on-reset threshold.
Could you let me know why TPS7A66…
Part Number: TPS7A66-Q1 Hi Team,
My customer is using TPS7A6650-Q1 to generate supply voltage (5V) for the microcontroller.
Can you please tell me if there is any possibility of output exceeding 5V +/-2% specification mentioned in the datasheet?
Please…
Part Number: TPS7A66-Q1 Hello,
My customer would like to know what is the EN pin sink current at V(en) = 3.3V? The datasheet specifies 1uA max at V(en) = 40V. Would the sink current scale down proportionally with lower V(en) voltage (for example, 3.3V…
Part Number: TPS7A66-Q1 Team,
The PSpice model on the TI’s website as ti.com showed is locked for certain version of PSpice to use.
Some of TI’s IC provided unencrypted one for simulating usage, so we would like to know if it is possible to share…
Part Number: TPS7A66-Q1 Other Parts Discussed in Thread: TPS7B81-Q1 , TPS7B81 Hi Team,
I have question about TPS7A66-Q1 pin function.
What is the function for SI/SO, I see the datasheet but it still confused me. Could you help brief introduce the function…
Part Number: TPS7A66-Q1 Other Parts Discussed in Thread: TPS7A02 Hello ,
Can you please tell me the input impedance at VIN pin?
I am connecting VIN pin to battery via a diode and my customer has requirement of high resistance between battery and GND(…
Part Number: TPS7A66-Q1 Hi Team, I have a customer asking about the injection current for TPS7A66-Q1. Are there reference available about this?
Thank you very much in advance.
Part Number: TPS7A66-Q1 Hi team,
A customer which has been using TPS7A6601QDGNRQ1 requests max. Iq at Io = 2mA .
Could you please provide the max. Iq data?
FYI. Datasheet shows only the Iq at Io = 0.2mA.
Thanks,
Sam Lee