Part Number: TPS7A69-Q1 I have pin 2 Si tied to the output with a 10K.
I have pin 7 So floating, it is open Drain.
Will this effect EMC performance or have any effect on the function or specs?
Will the output of So oscillate?
Why does the data sheet state…
Part Number: TPS7A66-Q1 Other Parts Discussed in Thread: TPS7A69-Q1 , Tool/software: Thermal Shutdown - "The purpose of the design of the internal protection circuitry of the TPS7A66-Q1, TPS7A69-Q1 is for protection against overload conditions, not as…
Part Number: TPS7A69-Q1 Hi team,
May I ask that do we have the P2P device to replace RENESAS ISL78307FBEAZ?
The attachment is the datasheet.
Thank you!
Regards,
Ivy
ISL78307FBEAZ datasheet.pdf
Part Number: TPS7A69-Q1 Other Parts Discussed in Thread: TPS7A66-Q1 , TPS7B84-Q1 , TPS7B85-Q1 Hi,
We are currently proposing the TPS7A69-Q1 as a p-p alternative to one of the competition part (CP).
One major difference is that the #CP has an additional…
Part Number: TPS7A69-Q1 Hi Team, Do we have the maximum power dissipation that the TPS7A69-Q1 can handle? We've seen the calculations of power dissipation in the datasheet but unfortunately there's no data of its maximum dissipation rating. Thanks…
Part Number: TPS7A69-Q1 Hi,
I am having problem to get the model of the TPS7A69-Q1 unencrypted. The model which is available in the product page is pspice encrypted format and it is not working with other simulation tools like tina or ltspcice.…
Part Number: TPS7A69-Q1 Hi,
Our customer is using TPS7A76950. When the chip's temperature is above 65 degree, the chip will enter high temperature protection mode and it doesn't work. And the high temperature will remain. After re-power on, the chip will…
Part Number: TPS7A69-Q1 Team,
I'm using the TPS7A6950-Q1 and don't need the PG function.
Can I let the pin floating in this case or are there any concerns?
Thanks and best regards,
B
Part Number: TPS7A69-Q1 Hello
I am planning to use the TPA7A69-Q1 (5V fix).
However my application has one concern.
Vin sometimes become 4.75V and output require 4.5V.
I looked 'Figure 9. Output Voltage vs Supply Voltage (Fixed 5-V Version, IL = 0)'…
Part Number: TPS7A69-Q1 Other Parts Discussed in Thread: TPS7A66-Q1 Hi Linear Regulators team.
Can we use Input-Voltage-Sensing option TPS7A66xx and TPS7A69xxx as a below?
I watch TPS7A66xx typeical application on datasheet as a below
However, We want…