Part Number: TPS7A7001 Hello,
We are using the TPS7A7001DDAR LDO in our design. We are providing a 5 V input supply to the LDO and obtaining a 3.3 V output, with an output load of approximately 420 mA. Could you please confirm the dropout voltage for…
Part Number: TPS7A7001 Tool/software: I would like to know about the LDO product TPS7A7001.The dimensions of the EXPOSED THERMAL PAD mentioned on page 19 of the datasheet are a maximum of 3.4×2.71. However, on page 23, it states a maximum of 3.1×2.40…
Part Number: TPS7A7001 Tool/software: Hi,
I am using TPS7A7001 2A LDO in the design where, input voltage is 5.5V and output voltage is 4V which is being used to power a variable load. It is observed that during high load consumption of 1.6A, LDO output…
Part Number: TPS7A7001 Hello
We are using TPS7A7001 in an application where Inrush Current of 4.2 A for 50 us is observed. Will this have an effect in the LDO over a long period of time.
I would also like to know the peak current the LDO can withstand…
Part Number: TPS7A7001 Dear TI Technical Support Team,
I am currently performing a Worst-Case Circuit Analysis (WCCA) for a 3.3V power rail design using the TPS7A7001DDAR .
I have encountered a significant output voltage deviation issue when considering…
Part Number: TPS7A7001 Tool/software: Hi Ti expert,
My customer wants to use TPS7A7001 under the condition of 6.5V in, 6.2V or 6V/2A out. Is it ok?
I can not find the maximum output voltage value in the darasheet.
And I see Vdrop is 380mV when output…
Part Number: TPS7A7001 Tool/software: I'd like to know about the LDO product TPS7A7001. The Dropout voltage written on page 6 of the datasheet is a maximum of 380mV. However, in Figures 3 to 5 on page 7 it is less than 150mV. Other than temperature and…
Part Number: TPS7A7001 Tool/software: Hi,
I am using TPSTA7001 LDO in my design and referring to the datasheet for selecting feedback resistors. The datasheet recommends choosing R2 between 27K and 33K when setting the output voltage.
I would like…
Part Number: TPS7A7001 Other Parts Discussed in Thread: TPS7A7100
Hi team,
In the functional block diagram of TPS7A7001, the device has UVLO block.
However, UVLO threshold or functionality are not described in the datasheet.
Could you please…
Part Number: TPS7A7001 Dear Sir,
I read TPS7A7001 datashhet and found R θ JA is 46.4°C/W, R θ JC(top) is 54.2°C/W. I am not sure if R θ JC(top) is error or not. Why R θ JC(top) value is bigger than RθJA one?