Part Number: TPS7A7002 Data sheet www.ti.com/.../tps7a7002.pdf lists thermal resistance Junction to board as 29.9 C/W, and J to C (bottom) as 6.9 C/W. I am using the 29.9 C/W value in my 2-resistor model for thermal simulation. Is this value correct?…
Part Number: TPS7A7002 Other Parts Discussed in Thread: TPS7A7300 What is the typical output noise voltage (10Hz to 100kHz) when operated with output of 5V and 3A?
Also, what is the PSRR when operated with the same output conditions?
Part Number: TPS7A7002 Other Parts Discussed in Thread: DAC5311 Hi,
I found nice (with all equation) example of controlling LDO output voltage with DAC voltage...
https://e2e.ti.com/blogs_/archives/b/precisionhub/posts/give-your-voltage-regulator…
Part Number: TPS7A7002 Hi Team:
In the databook ,it says “ For output capacitors larger than 47 μF, a feedforward capacitor of at least 220 pF must be used ”
The feedforward capacitor is connected from IN to OUT?
Any type or ESR requirements for…
Part Number: TPS7A7002TPS7A7002
Team
My customer have two technical problem as below and attached file.
Pls check the issue and let me get solution.
1. output voltage is 1V when TPS7A7002 was disabled
a. Output voltage of competitor(AP7176…
Part Number: TPS7A7002 I'm considering TPS7A7002 PCB board layout.(TPS7A7002.pdf P21)
With use stencil thickness of 0.1mm,Power pad solder Stencil Opening is 3.3mm(X)×2.6mm(Y)
On the other hand,Power pad geometry is 3.1mm(X)×2.4mm(Y)
Is it means…
Part Number: TPS7A7002 Other Parts Discussed in Thread: TPS7A92 , TPS7A84A Dear TI,
Is there any problem for output capacitance over 200uF.
I intend to use this IC as a cellular module power supply and manufacturer recommended 2mF input capacitance…
Part Number: TPS7A7002 Hi LDO team,
If I connect my negative supply to the ground pin of the LDO and my ground to the input of the LDO, the resulting output will be negative - correct?
What are the design challenges to consider? And how do I handle…
Part Number: TPS7A7002 Other Parts Discussed in Thread: TPS7A92 , , TPS7A7001EVM-065 , TPS7A53-Q1 , TPS7A84A Dear TI,
The present output voltage does not fall. (Maintain 1V)
To solve this problem, we tested the output with a pull-down resistor. (1K…