Hi Nick,
Yes, they found 2 units with this issue after the test. They put their board into the Champer for two hours under -40C to test the power sequency of each power rail. After about 2 hours, they took the board from the Champer. When the temperature…
Part Number: TPS7A8101-Q1 Other Parts Discussed in Thread: TPS748A-Q1 , TPS7A21-Q1 , TPS785-Q1
Tool/software:
Hi LDO Team,
May you have a good day!
My customer consider using TPS7A8101-Q1 for RF power, but we notice this is an old device, do we have newer…
Part Number: TPS7A8101 Hello,
The TPS7A8101 datasheet contains the following description of the noise characteristics. Low noise: 23.5uVRMS typical (100 Hz to 100kHz)
I am wondering what kind of measuring instrument was used to evaluate these values. I…
Part Number: TPS7A8101-Q1 hello,
May you let me know the internal ESD diode's reverse current capability? It's used for ICT purpose to detection the solder connection, i think it shall survive with few mA, saying 1.5mA. pls confirm, thanks.
…
Part Number: TPS7A8101 Hi,
I am confused by the plots from Figure 15 to Figure 18 in the datasheet. What is the difference between Figure 15/16 and Figure 17/18?
Is it possible to calculate the loop bandwidth of TPS7A81 when its output voltage is 5V…
Part Number: TPS7A8101-Q1 Other Parts Discussed in Thread: TPS7A8101 Hi Expert
we want to evaluate TPS7A8101 quiescent power but i doesn't find it in the datasheet.
I just found IGND, so could you please tell me which parameter can get quiescent power…
Part Number: TPS7A8101 I hav ea question about thermal pad of TPS7A8101.
Its thermal got nose sticking out in this SON (8) package.
The datasheet shows an example land pattern and it's better following this example pattern.
My question is what if…
Part Number: TPS7A8101 Other Parts Discussed in Thread: TPS7A89 , LP5907 , TPS7A47 , TPS22910A , TPS62913 Hello Team,
can you provide the max reverse current, please? If Vin drops down to zero volt rapidly the body diode may see too much current source by…