Part Number: AWR1843AOP Other Parts Discussed in Thread: TPS7A88 , TPS7A8101-Q1 , LP5907-Q1 , TPS796 , TLV713P-Q1
Hi Team, May I ask for help? Our customer have a concern: They are interested in the awr1843aop and they would like to make a prototype…
HI Ander,
The automotive version of the TPS737 was only released with a fixed 1.9V and fixed 3.3V versions. The non-automotive grade device has more options including adjustable. If you need an automotive grade 1A LDO, we do have the TPS7A8101-Q1…
Part Number: TLV320AIC20K Dear TI experts,
My customer drew their schematic with TLV320AIC20K. Could you review this schematic?
TLV320AIC20K.pdf
And one more question ;
They have audio interfaces of MCLK, SCLK, LRCLK, DATA OUT, DATA IN. All pins…
HI Vito,
The closest device we have that is released for Automotive grade is the TPS7A8101-Q1. Note: The Rohm device accuracy is at 25C our accuracy is over Line, load, and temperature. Meaning from the full input voltage (2.2-6.5V), load current …
Part Number: TPS7B7702-Q1 Other Parts Discussed in Thread: TPS7A8101 , TPS7B7702 Hi Expert
For load regulation and line regulation:
test condition: VI = VO + 1.5 V to 40 V and VI ≥ 6 V, IO = 10mA, voltage variation on FB pin and result is 10mV…
Part Number: TPS7A88-Q1 Other Parts Discussed in Thread: TPS82140 , Hi team,
Some power IC datasheet will have the Thermal Derating Curve which will show how the output current/output power change when temperature rise.
For example,tps82140 has the…
Hello John,
Please find my reply below:
>> 1) Figure 1 on page 4 refers to an LDO, TPS74801, in the EVM's. The schematics I have for both the AWR1642BOOST and AWR14243BOOST (Rev A) >>show this as a TPS7A8101, is this a newer revision of schematics…
Part Number: AWR1642BOOST Other Parts Discussed in Thread: AWR1642 , IWR6843 , TIDA-010022 i am trying to work on peoples counting project with awr1642 and two cc1352 boards. i found a document attached below of peoples counting project. it shows that…
Part Number: AWR1642BOOST Other Parts Discussed in Thread: AWR1642 , mmwave_radar_in_ADAS_applications.pdf
Hi TI Team,
Can you please let me know, if the BEAM formation of AWR1642 is like the attached image(circled in Black Color)?.
Is the AWR1642…
Part Number: IWR6843 Other Parts Discussed in Thread: IWR1843 , , AWR1843 , IWR1843BOOST Dear team,
I have some questions about the mmWave Radar IWR1843 and IWR6843.
1. Since I am working on enabling beamforming for the radar, I am looking for a way…