Part Number: TPS7A83A Other Parts Discussed in Thread: TPS7A8300 , Team,
TPS7A8300ARGW datasheet is missing the dimension for thermal pad, thus we are stuck at make the footprint.
Thank you for your fast support.
Kevin
Part Number: TPS7A83A Customer is using TPS7A8300A with Vin=1.5V, VBIAS=3.3V. EN is tied to PG from another DC-DC, with a 3V logic level. Is this allowed (EN>Vin)? Absolute Max spec (6.5V) would seem to say yes, Recommended operating spec would seem…
Part Number: TPS7A83A Hi Team, Our customer is requesting for the complete PCB land pattern information for TPS7A8300ARGWT (RGW (S-PVQFN-N20)). The customer informed us that the Footprint information of RGW 20 pins in the ultralibrarian is taken from RGR…
Part Number: TPS7A7001 Other Parts Discussed in Thread: TPS74801 , TPS7A83A , TPS56637 Hi all
My customer has this specification for an LDO: Vin=3.4V, Vout=3.3V, Iout=1A and he preselected the TPS7A7001.
Looking at the Datasheet I find this is marginal…
Part Number: TPS7A83A Other Parts Discussed in Thread: TPS7A8300 , Hi team,
whether the device TPS7A8300 and TPS7A83A can be used for below application?
3.3v input 0.9v output, Iout=0.63A, Tamax=55°C. RGW package is fine. Thanks.
Part Number: TPS7A83A Hi ,
Here is a question on TPS7A83A Vout short protection.
In customer side, there is a DCDC as input of the TPS7A83A. Then when Vout of TPS7A83A is short, then Vout of DCDC also drops.
Current Cout of TPS7A83A is 2x22uf. Then they…
Part Number: TPS7A8300 Other Parts Discussed in Thread: TPS7A83A Hi Team,
Is it OK to assume that the dropout voltage characteristics of TPS7A83A and TPS7A8300 are the same?
My customer asked that
The dropout voltage graph described in the TPS7A8300 data…
Part Number: TPS7A83A Hello Team,
May I confirm with you that with no external bias, the correct connection of bias pin is floating or connecting it to a capacitor?
In Figure 48. ANY-OUT Configuration Circuit (no external bias) the bias pin connects…
Part Number: TPS7A83A Hi Team,
Customer would like to see the real test data with their condition to make sure no problem for Vdropout, and output noise and PSRR performance. Would you please help to verify and note what's the proper Cnr/ss, Cff, and…