Part Number: TPS7A87 Dear team,
I measured PSRR of TPS7A87 based on TPS7A87EVM these days, and I found that the result is close to the value of datasheet in 10Hz-100KHz, but the peak value is 20dB in 1MHz-10MHz, which is much lower than that of datasheet…
Part Number: TPS7A87 Dears:
Could you kindly help to check the schematic issue about TPS7A87?
TPS7A87&90.pdf
Is there any issue about the schematic?
Thanks a lot!
Best regards!
Luck Wu
Part Number: ADS1256 Other Parts Discussed in Thread: OPA350 , REF5025 , REF6025 , REF5050 , , REF6050 , TPS7A87
Here's my 2.5V VREF and 5.0V AVDD circuit base on other post ,
but I am not sure how to define these passive components. Any comments?
Part Number: TPS7A87 Team,
Our customer has much interest for TPS7A87, but also has some concerns about cross talk between 2 channels.
Could you share any information/material ? Or could you give any guideline for this ?
よろしくお願いします。
Thanks and Regards…
Other Parts Discussed in Thread: TPS7A87 , TPS7A89 , TPS7A88 Hello,
Can I get the TPS7A87EVM and the TPS7A89EVM? I found that the TPS7A88EVM but there is no EVM for TPS7A87 and 89.
Should we replace the device on the TPS7A88EVM?
Best Regards, Ryuji Asaka
Hi Stefano,
TLV751 or TPS7A87 would be the best selections here. TPS7A87 brings more low-noise performance whereas TLV751 is a bit smaller but has lower Iq. Both have separate enable pins for you to use.
regards,
Wilson
HI SHH,
A p2p for the MM3816 could be the TP7A03 . Even though this is a low I Q LDO, it does have a phenomenal load transient response. Another option could be the TLV740 . Both are Pp2p.
We don't have p2p for the MM176 but the TPS7A90 could be a…
Hi Seongdae,
TLV755P for fixed VOUT device. We offer the 2x2 WSON package for good thermal performance, and also offer the 1x1 WSON for space constrained designs
TLV751P as a dual output LDO in a 2x2 WSON package. Great option to consolidate board space…
Hi Shmuel,
Here are the packages the TPS7A20 is expected to come in. Will either of the other packages for the TPS7A20 work for you?
X2SON: 1mm x 1mm
DSBGA: 0.603mm x 0.603mm
SOT23-5: 2.90mm x 1.6mm
My colleague also suggests the TPS7A87 for a duel channel…