Part Number: TPS7A92 Other Parts Discussed in Thread: TPS7A90 Hi team We are using TPS7A92, can we please suggest an alternate part in same footprint having lower Junction to Ambient resistace
Part Number: TPS7A92 Hello,
I would appreciate your support in responding to the customer's question regarding the subject above.
This topic involves ESD testing, and I would like to share the customer's questions along with details of the ESD test…
Part Number: TPS7A92 Figure 14 on the datasheet shows dropout voltage vs. output current for VIN = 5.5V. I;m looking for this same plot for VIN = 3.3V (or as close to 3.3V as possible).
Part Number: TPS7A92
Hi, Are the below circuits correct for the output voltages of 1.8V and 1 V respectively? Please let me know if I am missing anything else.
Output Voltage: 1.8V
Output Voltage: 1V
Part Number: TPS7A92 Tool/software: The data sheet for the subject device shows a MAX height of 0.8 mm. Can you provide a minimum height?
Thanks,
Stuart Wallace
Part Number: TPS7A92 Tool/software: Hi team,
Could you please help to confirm which parameter should be used to estimate the temperature rising if I know the power consumption based on Vin/Vout/Iin/Iout?
BRs,
Rannie
Part Number: TPS7A92 Hi,
I'm planning to use TPS7A92 for my project,
this is my requirement,
Vin=5V
Vout = 3.8V
Iout = 1.6A
Ta= 70C
based on datasheet, i have done some calculations,
part has RθJA = 56.9 °C/W, if we calculate the…