Part Number: TPS7A94 Tool/software: Hi Sir,
Regarding the output from TPS7A94 device, we need 0.5V output, but i am getting 2.2V.
I have used below schematic diagram for the reference.
I have changed the R6 value from 22k to 3.3K for the output…
Part Number: TPS7A94 Tool/software: HI team,
TPS7A94 Ic is not available in webench power simulation library.
Is there any other way to simulate this part in webench power designer.
Part Number: TPS7A94 Hi team,
In the below thread, the statement that “fast charge-up switches to a 150 µA internal current source when PG_FP reaches 93% of the intended Vout value” is a typo.
https://e2e.ti.com/support/power-management-group/power…
Part Number: TPS7A94 Tool/software: Hi!
I used to have in my designs low-noise high-PSRR LDOs from AD, but I want to try your product.
I see TPS7A94 uses pretty the same technique as LT30xx family, in this case I want to replace LT3041.
My question…
Part Number: TPS7A94 Tool/software: Hi All,
We need to reduce space and component count around EN_UV pin. We want to avoid resistor divider tied to this pin (as recomended in datasheet). Is it possible to connect as follows? If not, why?
Input voltage…
Part Number: TPS7A94 Tool/software: Hi Team,
Base on formula RFB_PG(TOP) = RFB_PG(Bottom) x (VOUT (nom)/0.2V x K - 1)
Vin:5V; Vout:3.3V
The required output voltage is VOUT (nom)=3.3V (set according to Table 8-1) RFB_PG(Bottom)=12.4K (set according…
Part Number: TPS7A94 I wired-up this Low-Dropout regulator per the Typical Application Circuit on page 49 of the datasheet Figure 8-27, and set the resistor for pin 7 to 26.7k ohms which should set the output voltage to 4.0V, I am getting 4.7V out and…
Part Number: TPS7A94 Other Parts Discussed in Thread: TPS7A96 Tool/software: Hello.
As I was reading the datasheet, I find some connection errors in the typical application shown in the datasheet below. The PG pins should not be grounded. The datasheet…
Part Number: TPS7A94 Tool/software: Hi team, Datasheet says EN-UV max rating is Vin. But the datasheet doesn't specifically say you can connect EN to Vin. Are we able to tie that EN_UV pin directly to Vin if not used? Or do we need at minimum a series…
Part Number: TPS7A94 Tool/software:
Hi All,
I needed a review for my schematic and layout (images attached). I want the output of the LDO to be 0.6V with a supply voltage of 5V. (As the output voltage is less than 1.2V, the current limit is set to…