Part Number: TPS7A94EVM-046 Other Parts Discussed in Thread: TPS7A94 , TPS7A57 Hello,
I am wondering if the TPS7A94 can output high-Z when no input voltage is supplied. I measured 100mA current draw when supplying 1V to the output BNC connector in the EVM…
Part Number: TPS7A94EVM-046 Hi Team,
A customer has a question regarding the capacitor selection for the EVM.
What is the reason for putting two types of 10uF on the PCB?
There are 25V (1210) types and 16V (0805) types.
Why is the 25V type used here? …
Part Number: TPS7A94EVM-046 Hi,
I looked at the user's guide of TPS7A94EVM-046,
The PCB Layout on page 5 and 6, I can't find out input BNC connector to
Device input connection.
I found device to J3-1,2 input trace has stub, so I guess input polygon…
Part Number: TPS7A94 Other Parts Discussed in Thread: , TPS7A57 Hi,
A question: the TPS7A94 datasheet does not provide a specific amount of copper needed for thermals so the device runs cool enough to hit the current spec.
The TPS7A94EVM-046 board has…
Part Number: TPS7A94 Hi ,
According to TPS7A94 data sheet, PG supposed to be pulled up to VIN.
The TPS7A94EVM-046 has PG pin pulled up to VOUT.
As it works logic flag of power good, VIN and VOUT does not matter while
the logic level works OK??
Thank…