Part Number: TPS7B68-Q1 Hi Jason,
My customer asked additional question regarding to input capacitor for TPS7B68-Q1.
They want to use electrode cap with below spec.
- 100uF
- ESR=0.9ohm(100kHz@25degC), 14ohm(100kHz@-40degC)
Is there any concern in terms…
Part Number: TPS7B68-Q1 Hi team,
My customer do not need Watchdog timer function.
Could you tell me how to connect the pins which is relative watchdog as WD, WDO, WRS, WTS, WD_EN?
Regards,
Yoshi
Hi Luke,
We don't have any LDOs that communicate through SPI. The devices in our portfolio with watchdog are TPS7B63-Q1 , TPS7B68-Q1 , and TPS7A63-Q1 . Of these, the TPS7B68-Q1 is the only one that meets the 500mA requirement.
Regards,
Nick
Part Number: TPS7B68-Q1 Dear all,
I would like to check about title.
Witch should I connect NC pin to GND or floating? Witch is better? Are both same condition?
Best regards,
Part Number: TPS7B68-Q1 Dear all,
Could you teach about the driving capability of PG and WDO?
Do you have VOL vs IOL graph?
It is OK that the data is test result, but please teach about the test condition.
I am looking forward to hearing from you as…
Part Number: TPS7B68-Q1 Dear all,
Which does the configuration of theta-ja test board is 1s or 2s2p?
I would like to know the test condition how you confirmed 37.8C/W.
Best regards,
Part Number: TPS7B68-Q1 Dear all,
Could you check my pin connection idea?
Please see attached file.
* I will use this device with standard WD and without power good.
3288.circuit diagram.pdf
Best regards,
Part Number: TPS7B63-Q1 Other Parts Discussed in Thread: TPS7B68-Q1 Hi team,
Do you have "Pin open-circuited" Pin FMEA especially for "/WD_EN"? Lower link does not include that.
TPS7B63xx-Q1 Functional Safety FIT Rate and Failure Mode…
Part Number: TPS7B68-Q1 Dear all,
Could you teach me the recommended value of pull down resistor?
We think to use WD_EN as always enable during normal operation, and disable during pre-shipment inspection.
And we think to connect this pin like following…
Part Number: TPS7B68-Q1 Dear all,
I found that typo in Fault 2 taxt at data sheet page 20.
You described that 'WDO is triggered after the maximum open-window duration t(WD) / 2.', but this duration should be 't(WD)'.
Is my understanding…