Part Number: TPS7B68-Q1
Hello,
Please answer following question from customer.
Q1: V(PGADJ_TH)
Please advise, if following V(PGADJ_TH) min, typ and max voltage will change linked to Vout voltage or these values are constant in spite of Vout is 4.9V…
Part Number: TPS7B68-Q1 Dear all,
Could you teach us what peripheral elements is needed when we do not use power-good and use standard watch dog?
My idea of peripheral elements are following. Is this correct?
pin 1[IN]: Input capacitor
pin 4[EN]: no (connect…
Hi Tomo,
Both TPS7B82-Q1 and TPS7B68-Q1 are AEC-Q100 qualified devices.
The targeted applications for TPS7B82-Q1 are:
The targeted applications for TPS7B68-Q1 are:
We do not share how our customers use our LDOs in their applications without their explicit…
Hi Hideyuki,
Unfortunately we do not have any plans of adding additional package variations of the TPS7B67-Q1. I would encourage you to look at TPS7B68-Q1 as an alternative to the TLS850 as the TPS7B68-Q1 does have a watchdog timer and will have lower…
Part Number: TPS7A19 Other Parts Discussed in Thread: TPS7B82-Q1 , TPS7B68-Q1 Dear Sir:
We used TPS7A19 for motorcycle application. It Vin is 12V from the lead-acid battery and Vout 5V to MCU. When we start the engine at moment, 12V will drop under…