Part Number: TPS7B84-Q1 Other Parts Discussed in Thread: TPS7B69-Q1 Hello Team,
I am looking for equivalent part for TPS7B84-Q1.
Requirements: 3.3V fixed output with 10mA peak, 2-5mA steady current. Quiscent current is lesser than 50uA.
Cost is the main…
Part Number: TPS7B69-Q1 HI,
TPS7B6950QDBVRQ1, Input short circuit test (Vin&GND),IC is broken,no output 5V, What is the reason? What are the good improvement measures
The IC was tested many times and broke every time.
Input capacitor is 10uF, Output…
Part Number: TPS7B69-Q1 Hi
Regarding to TPS7B6950QDBVRQ1, it would regulate output voltage to 5V when input voltage is 24V.
If input voltage is 24V and GND is float, what voltage appears at OUT and GND pins respectively?
Or internal FET would be opened…
Part Number: TPS7B69-Q1 Other Parts Discussed in Thread: TPS7B69 , LM2937 , Please help to support load transient and line transient compare wave form at TPS7B6950-Q1 and LM2937-5.0,I can’t easy get it from each spec.
Test condition :
Vin 16 to 36V…
Part Number: TPS7B69-Q1 Hi, my customer is using subject part.
Lead finish for this part is Tin Over Copper lead frame. Could you please let me know whether the Tin is “Matte” or “Bright”
Part Number: TPS7B69-Q1 External Vout of 3.3V is applied to TPS7B6933-Q1 without any Vin. This is for MCU programming at assembled PCB. Reverse current can flow through internal body diode. How to protect TPS7B6933-Q1 in that case? Is there a maximum possible…
Part Number: TPS7B69-Q1 Other Parts Discussed in Thread: TINA-TI Tool/software: TINA-TI or Spice Models Hello Team,
Do we have available TPS7B6950-Q1 model compatible with TINA. my customer is not able to use Pspice model in TINA.
Regards,
Mahendra
Part Number: TPS7B69-Q1 Hi team,
Would like to check if TPS7B6933-Q1 (3.3V fixed) can have output cap lower than 2.2uF, e.g. 100nF only? The max output current is only up to 1uA and customer understands we recommend cap from 2.2uF to 100uF but customer…
Part Number: TPS7B82-Q1 Other Parts Discussed in Thread: TPS7A25 , TPS7B69-Q1 , TPS7B81-Q1 Hi Team
Customer is looking for the replacement of TPS7B8250QDGNRQ1
(do not need P2P , just need same function)
And the target price is 0.1 USD!
I watched around…
Part Number: TPS7B69 I want to confirmation the power-up timing of TPS7B6933-Q1.
The data sheet of TPS7B6933-Q1 has the following description. ------------------------------------------------------------ During the initial power up, the regulator has a…