Part Number: TPS7B7702-Q1 Hi,
From datasheet, we know that "Each time the LDO switch is enabled on the rising edge of the EN pin or during the exiting of the thermal shutdown, the short-to-battery detection occurs. At this moment, if the device detects…
Part Number: TPS7B7702-Q1 Other Parts Discussed in Thread: TPS7B7702 Hello:
Regarding the TPS7B7702 chip, I have a question to ask
Can the EN2 SENSE2 LIM2 FB2 OUT2 pins of the chip be suspended when not in use, or what should be done
Part Number: TPS7B7702-Q1 Hi Team,
We are using the TPS7B7702-Q1, we are very care about the Rja data, the application is the automotive. So we plan to design a resistance test board to double-confirm the Rja data just like datasheet said, to make sure…
Part Number: TPS7B7702-Q1 Other Parts Discussed in Thread: TPS7B7702EVM , Hi Team,
We are using the TPS7B7702EVM to power the Car Antenna, but we find the EVM have a 1mH inductor between the LDO output and Antenna, is it mandatory?(for the real application…
Part Number: TPS7B7702-Q1 Hello Expert,
We'd like to confirm EN1/2 and sense1/2 pin status when Vin is removed? Could you please provide this information?
I suspect that it is Hi-z but I'd like to make sure about it.
Best regards, Kazuki Kura…
Part Number: TPS7B7702-Q1
Hi, Support Team we will use TPS7B7702-Q1, and output setting 4.7v. if output short to 5V or 6.5V, have any alert to protection?
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence
Part Number: TPS7B7702-Q1 Hi Team,
I have some questions:
Currently, TPS7B7702-Q1 5mA has an accuracy above 5mA. What is the accuracy below 5mA?
Is there any information related to the accuracy test of TPS7B7702-Q1?
Thank you so much.
Part Number: TPS7B7702-Q1 Hi
I'd like to know the Min and Max values for Rsense.
The output current of the circuit I designed was 4 mA, so I applied Rsense as 47K.
Is there any problem?
Part Number: TPS7B7702-Q1 Hello~
I have a few questions regarding the use of the TPS7B7702-Q1 device.
1. The output is disabled in the failure mode indicated in red in the picture below. In this case, are the outputs of both channels disabled?
2. what…
Part Number: TPS7B7702-Q1 Hi team,
My customer wants to use TPS7B7702-Q1 to output 2 supply rail. However, they do not have much ADC resource, they do not want to connect the sense pin to ADC.
Now they only want to know the short circuit fault. They connect…