Part Number: TPS7B82-Q1 Dear:
please help me check the schematic is ok ? however , in the end customer, found the chip burned and the output cap.C738 short as attached,the customer changed the new chip , it is ok;
Could you help me analysis the reason…
Part Number: TPS7B82-Q1 Hi Is there anywhere inteh data sheet or teh TI ordering system that identifies what teh ordering part number is- clearly teh 33 is 3.3 and 50 is 5V by observation, but I cant see it written down anywhere
Part Number: TPS7B82-Q1 Other Parts Discussed in Thread: TPS7A61-Q1 , TPS7B70-Q1 , TPS7B63-Q1 , TPS7A65-Q1 , TPS7B81-Q1 , TPS7A66-Q1 Hi
I would like to ask 2 questions below:
1. TPS7B8233 only supports 3.3V output and TPS7B8250 only supports 5V output right…
Part Number: TPS7B82-Q1 Hi team,
I believe this LDO has a brick wall type current limit function. My customer wants to know the response time of the current limit.
Once the device goes into the current limit region, how long does it take to start limiting…
Part Number: TPS7B82-Q1
Hi,
We are using TPS7B8250QDGNRQ1 in the design. Please provide response for the below queries,
1)On pg 7, the current limit is provided as 510mA. In our design, if the output is getting shorted, then we are getting the junction…
Part Number: TPS7B82-Q1 Hi team,
In the case that the output is shorted to GND, the device continues the current limit and the thermal shutdown cycle repeatedly.
If this condition continues, does it cause a damage to the device?
It looks the TSD(max)…
Part Number: TPS7B82-Q1 Does the leakage current on EN, which is indicated as max of +/-0.003uA in the following thread , have any dependence on temperature?
Is this factored into the above mentioned max leakage?
Part Number: TPS7B82-Q1 Hi,
I would like to check with you if TPS7B8250-Q1 in SSOP package will be able to dissipate some pulses of load current.
Load profile here is to supply an RF module which consume around 300mA during 100us every 1ms.
The ambient…