Part Number: TPS7B82-Q1 Dear,
our client spec:
VIN=24V~30V
Iout=250mA
Vout=3.3V
we find TPS7B82-Q1 maybe can meet spec, but how to setting output current?
If any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence.
Part Number: TPS7B82-Q1 Hello Team,
What is the maximum current that Enable pin of TPS7B82-Q1 can sink?
I am not able to find this information in datasheet.
Regards,
Mahendra
Part Number: TPS7B82-Q1 Hello ,
I am using TPS7B82-Q1 as 5V regulator, can this device will support to withstand ISO7637 part 2 automotive transient pulses 1, 2A, 3A and 3B etc. Also if testing is done, I need to know the specs of the pulse for which…
Part Number: TPS7B82-Q1 Team,
From TPS7B8250QDRVRQ1 datasheet, R_theta_J_A = 63.9 C/ W (for HVSSOP), 72.8 C/ W (for WSON). And there is thermal pad in the IC package, my question is if we use that thermal pad for heat sinking how the R_theta_J_A number…
Part Number: TPS7B82-Q1 Hi team,
The datasheet showed minimum input voltage is 5V + VDropout as below.
I think the TPS7B8233 is 3.3V + VDropout. Is it correct?
Regards,
Yoshi
Part Number: TPS7B82-Q1 In spice simulations with the TPS7B8233-Q1 part, after the part went into undervoltage shutdown at 2.7V the part started to sink current. The current going into the device spikes to 20mA then decays. Is this to be expected from…
Part Number: TPS7B82-Q1 Hi team,
I noticed on the datasheet, the Enable input voltage is 0-Vin range. However, i got a bit confused about the logic-input high/low level below.
Is this like a hysteresis? Or how to understand here?
Thanks a lot for your…
Part Number: TPS7B82-Q1 Hello,
page 1 of datasheet mentions "Stable with low-ESR Ceramic Output-Stability Capacitor".
This could be misleading. Do you require ceramic capacitor for stable operation of LDO ? Or is Electrolytic cap or other types…
Part Number: TPS7B82-Q1 Dear sir,
we are having 15V input voltage and by default we are getting 3.3V as output voltage.
How to change the output voltage to 5V? Kindly guide us to change the output voltage.
Thanks & regards,
Rajasekaran.
Part Number: TPS7B82-Q1 Other Parts Discussed in Thread: TPS7B7701-Q1 , TPS7B4253-Q1 Hello,
Oour customer is looking for an automotive 12Vtyp, 36Vmax input to 6V/300mA output, low Iq <2uA LDO and TPS7B82-Q1 is the most appropriate device. However the…