Part Number: TPS7B84-Q1 Hello expert, This is just confirmation but I'd like to ask you just in case.
Our customer's use case for this device include dropout operation mode. I measured loop performance by FRA but I cannot observed expected waveform…
Part Number: TPS7B84-Q1 Hello expert,
I have question for TPS7B94-Q1's output capacitor. This device's datasheet required they need to place 2.2uF output from the point of view of stability but they can use 0.1uF if they add electrolytic capacitor…
Part Number: TPS7B84-Q1 Hello Expert, Our customer considering to use this device. Then, I receive questions as below. Would you answer following questions?
Does datasheet's "Regulated output" include not only reference accuracy but also line and load regulation…
Part Number: LM63615-Q1 Other Parts Discussed in Thread: TPS7B84-Q1 Hello, Experts,
We have a question about the back PAD soldering joint area; Do we have a recommended joint area ratio excluding void?
Best Regards, Masaru
Part Number: TPS7B84-Q1 Hi experts,
May I know whether below plot is for adjustable or fixed 5V part? Customer want to know the IQ difference between TPS7B8401 and TPS7B8450. Do you have that data? What's the value of the internal feedback resistor for…
Part Number: TPS7B84-Q1 Hi team,
Could you advise how does the device behaves in the conditions below?
This is the automotive application.
BATT=9V to 16V
IN
GND
出力
1
BATT
GND
BATT
2
BATT
GND
GND
3
Open
GND
BATT
4
Open
GND
GND
5
BATT
…
Part Number: TPS7B84-Q1 Hi Team,
Can you confirm the TPS7B8480QWDRBRQ1 orderable has a fixed 8V output. There is some confusion because the datasheet states that there is only fixed voltages of 3.3V and 5V.
Best,
David
Part Number: TPS7B84-Q1 Hi team,
I have a question about VIN power up slew rate and POR of this device.
1. Is there a requirement in power up slew rate for VIN? In my case(automotive), there is a case that takes about 30seconds to power up.
Is there any…
Part Number: TPS7B84-Q1 Hi teams
Customer is using TPS7B84-Q1 adjustable output version in their project. They noticed that the maximum output voltage in datasheet is 18V (Shown in below diagram)
They want to know why we this part can't output a voltage…
Part Number: TPS7B84-Q1 Hi Expert,
When input voltage is 3.3V,output voltage is 3V@100mA,how much is the dropout voltage. In the datasheet, only spec with Vout>3.3V is shown.
Thanks
Elec Cheng