Part Number: TPS7B85-Q1 Tool/software: Hi TI experts:
I want to confirm that if I don't use SI(sense input) and PGADJ(Power-good threshold-adjustment pin) monitor function. How to handle these pin? Floating or grounding to GND?
Looking forward…
Part Number: TPS7B85-Q1 Other Parts Discussed in Thread: TPS7A69-Q1 , Hi, Team,
What is the spec difference between TPS7A6933-Q1 and TPS7B8533-Q1? Why is the price of x6933 is times of higher than x8533? Is x6933 not our hero device any more?
Thanks~
Part Number: TPS7B85-Q1 Hi
Regarding the input capacitance of the power supply IC, we are considering placing two 0.1uF MLCCs in series and a 1000uF electrolytic capacitor on the IN terminal line.
The data sheet states min0.1 uF, typ 1uF, and contains…
Part Number: TPS7B85-Q1 Hello team,
I am looking for the below LDO.
1. >100mA
2. Small Package
3. Low Iq during EN=High (system needs 5V even in system sleep mode)
4. with PG
Most suitable part is TPS7B85-Q1?
If so, and If SI and SO is not used in…
Part Number: TPS7B85-Q1 Hi Team,
I read the datasheet of this device and it does not mention what to do if SI pin is unused. Should I keep it floating or connected to GND? Is it possible not to use sense?
I hope you can help clarify.
Regards,
Marvin
Part Number: TPS7B85-Q1 Other Parts Discussed in Thread: TPS7B86-Q1 I'm using our PSpice model to simulate the TPS7B85-Q1, but am confused with the FB pin being in the simulation, since it isn’t on the datasheet. I see this variant has a NC pin instead…
Part Number: TPS7B85-Q1 Hi Team,
I am not so clearly about the power-good part. For example, my customer want to monitor the output 5V and when it exceeds 5.2V, will trigger reset signal.
I am wondering if TPS7B85 can achieve this. Thanks!