Part Number: TPS7B92 Tool/software: For this LDO , The I/P volatge is 24V , Vout = 5V
How to calculate the thermal increase of the IC at these conditions :- @100 mA @150 mA @300 mA
Part Number: TPS7B92 Other Parts Discussed in Thread: TPS7B84-Q1 , TPS7E81 I have used 12V fixed LDO TPS7B92120DBVR but the voltages are not constant in every board. I have tested on 2 boards in one board the voltage level is 11.98 and in other board…
Part Number: TPS7B91 Other Parts Discussed in Thread: TPS7B92 , Tool/software: Hi,
May I know TPS7B91/TPS7B92 is made by 12" wafer?
Customer want to using newest process prodcut to have better price and avoid EOL risk.
Thanks!
Jeff
Part Number: TPS7B92 Tool/software: Hello LDO team,
Regarding the TPS7B92 the DS says that:
Available output voltage options:
Fixed: 1.2V to 12V
Adjustable: 1.205V to VIN − VDO
However I cannot see where the TPS7B92 with an adjustable…
Part Number: TPS7B92 Tool/software: Hi, I think you have a mistake in the datasheet. You write on page 3 that the input is pin 1, fb is pin 4 (if adjustable) and output is pin 5. But in your example pcb on page 28, you have fb as pin 1, input as pin 4…
Part Number: TPS7B91 Other Parts Discussed in Thread: TPS7B92 Tool/software: Team-
Would be really helpful to have a SPICE model for the TPS7B91.
Is one in the works?
Would plan to use it in TINA or QSPICE.
Thanks, -Steve
Part Number: TPS2116 Other Parts Discussed in Thread: TPS7B92 , TPS2117 Tool/software: Hi,
I'm developing an IoT solution that will be powered by two sources :
an input in the terminal block, with compatibility between 5 and 24V
1 or 2 lithium…