Part Number: TPS7H1101A-SP Other Parts Discussed in Thread: TPS7H1101-SP , Hello,
Could you please tell us what is different between TPS7H1101-SP and TPS7H1101A-SP?
Thank you.
JH
Part Number: TPS7H1101-SP Other Parts Discussed in Thread: TPS7H1101A-SP , TPS7H1101SPEVM To get more phase margin (above 30deg) I need to add 12 x 330uF caps on the output. Seems excessive. Need help to figure out how to get this number down.
Thanks.
Part Number: TPS7H1101-SP Hi Team,
The datasheet has the following statement: "For demanding load requirements, multiple LDOs can be paralleled". Is there a recommended configuration for paralleling three. I have 5V in and 4.5V out. This should…
Part Number: TPS7H1101-SP Other Parts Discussed in Thread: TPS7H1101A-SP Hi Team,
I need help with the thermal information of TPS7H1101-SP. can you provide the thermal resistance to the package top?
Regards,
Marvin
Part Number: TPS7H1101-SP Hello team -
We are interested with the CSR value, if we are using this device with different input/output voltage, and different load current from what the datasheet tested, would this number still valid? Is the CSR number…
Part Number: TPS7H1101-SP We’re doing a DPA on a 5962R1320201VXC (TPS7H1101-RHA). Per MIL-STD-883, TM 2018, SEM is not required for planar die. Is the die fully planar with no oxide steps? Are chemical mechanical polish (CMP) processes used? Or…
Part Number: TPS7H1101-SP Other Parts Discussed in Thread: TPS7H1101A-SP I am using four of the TPS7H1101A-SP LDOs on one of my boards and would like to get SPICE model to be able to run simulations in the LTSpice.
Thanks,
Imran Sharafat
Part Number: TPS7H1101A-SP Other Parts Discussed in Thread: PSPICE-FOR-TI , , TPS7H1101-SP Can we please add the TPS7H1101A-SP model to PSPICE-for-TI? At this time, only the WCA model is available in the default library.
We have a need for the transient…
Part Number: TPS7H1101-SP Hello:
Regarding Pin 9 " Power Good"
Will the regulator function normally if Pin 9 is left unconnected and not pulled high.
Thank you
Mark