Part Number: TPS7H1101A-SP Hello,
My customer wants to use TPS7H1101A-SP with the conditions below.
- VIN = 5V / VOUT = 1.5V / Room temperature
What is the maximum current available? How can they calculate it?
Thank you.
JH
Part Number: TPS7H1101A-SP
Hello,
Gain and Phase response from hardware does not match PSPICE model or TINA model sourced from TI's website. Worst Case Circuit Analysis (WCCA) is required for the project using this part. Hardware/Model verification is…
Part Number: TPS7H1101A-SP The datasheet states " It is not recommended to use overcurrent limit activation thresholds of less than 500 mA due to internal bias offset currents representing a larger percentage of total IPCL current and therefore additional…
Part Number: TPS7H1101A-SP Hi,
When I run AC analysis on the WCA PSpice project on the TPS7H1101A-SP product page, I get a 0 degree crossing around 750 Hz, accompanied by 49 dB of gain. See the attached schematic and Bode plot. I believe this would be…
Part Number: TPS7H1101A-SP I am also interested in the output voltage accuracy (+/-2%) and the impact of initial value, radiation, temperature and lifetime.
Could you help me with that ?
Thanks in advance,
Part Number: TPS7H1101A-SP Hello,
I am looking for a file that is compatible with LTSpice. These are some of the errors I get with the unencrypted model: (Also looking for transient analysis).
Questionable use of curly braces in "b§e_abmgate yint 0 v…
Part Number: TPS7H1101A-SP We have an unstable oscillation TPS7H1101A-SP on the bench.
We would like to use the TPS7H1101A-SP Pspice for TI model to bound the amount of oscillation amplitude we are seeing on the bench over lifetime.
1) I've used the …
Part Number: TPS7H1101A-SP Other Parts Discussed in Thread: TPS7H4001-SP , I did not find the "WCA model guide" referenced in the example worst-case analysis PSpice testbench, I'm wondering if there is one available for this part similar to this:…
Part Number: TPS7H1101A-SP Is there further information available about the parallel operation? Is there an excel sheet version of TPS7H1101A_DesignCalculator.xlsx configured for parallel operation? I am struggling to understand how to select RCL for the…
Part Number: TPS7H1101A-SP Hi,
In the datasheet it says to pullup the power good signal to the VOUT pin.
I have a case where this can't happen (multiple 7H1101 on the power good pin).
Does this requirement need to be met as long as I meet the input…