Part Number: TPS76901-HT Other Parts Discussed in Thread: TPS7H1201-HT Hi,
Is there any spice / macro simulation model available for the LDO TPS76901-HT ?. If not available could you recommend something that is the closest match ?.
The required input voltage…
Hello Tom,
I will look into this and get back to you. I believe the reason that E2E didn't recognize the part is you put the orderable part number instead of the generic part number (TPS7H1201-HT). Either way, I appreciate knowing the orderable number…
Hello Mike,
Sorry for the delay. Since our recommended operating range has 5V as the minimum input I have determined this IC will not work for your needs. The formula you initially mentioned is for use withing the operating range.
I would suggest looking…
Part Number: TPS76901-HT Other Parts Discussed in Thread: TPS7H1201-HT Design requires the 175C temperature spec, but the current drive is not within spec. The maximum output is 100mA, which is short by a factor of 2.5x. Is it possible to parallel connect…
Part Number: TPS76901-HT Other Parts Discussed in Thread: TPS7H1201-HT Hi all,
I’m not sure if this post should be here or in the power management group. However my application runs at 200 Deg C and is very space constrained.
I am looking for a…
Other Parts Discussed in Thread: TPS76901-HT , TPS7H1201-HT TPS76901-HT Specification is for 100ma output. I am having dropout at about 30 ma. My input voltage is 5 volts. Output 3.3V.
This regulator should perform at this output level from what I can tell…
Other Parts Discussed in Thread: TPS7H1201-HT , TPS7H1101-SP Greetings,
I'm looking at the TPS7H1201-HT, TPS7H1101-SP datasheet trying to make sense of the thermal information provided on page 7. Various thermal resistances are provided in the table for…
Hello Andrew,
I really appreciate your question here, because I am now stuck in the completely same scenario/question than you :)
I also looked forward to use the TPS76901-HT as an linear regulator at very high temps, but I can not use it
for my needed…
EL,
You may want to consider TPS7H1201-HT one of the latest offering from HiRel ( -55C to 210C) which has the input voltage range up to 7V and will easily meet your system needs to get 5V output. It also has thermally enhanced package. See attached link…