Part Number: TPS7H2201-SP Hi,
We are using 5962-1722001VXC part in our custom board. As per the datasheet, RJC(bot) is 0.6 and RJC(top) is 96.3. According to these values, it is clear that the heat flow from the component will be towards bottom of the…
Part Number: TPS7H2201-SP Tool/software: I am trying to run a transient analysis simulation for TPS7H2201-SP and when I click run, it shows the log and says the file path followed by "Expected directive or device instantiation here." What does that mean…
Part Number: TPS7H2201-SP Tool/software: Hi Expert,
Do we have any recommended 3rd party for lead forming about TPS7H2201-SP SDFP package?
Regards,
Kotaro Yamashita
Part Number: TPS7H2201-SP Other Parts Discussed in Thread: TPS7H2211-SP Tool/software: Hi, Do there exist a tweak that can make this IC work with negative input voltages ? BR, Mohamed
Part Number: TPS7H2201-SP Tool/software: I am looking for a part similar/identical to TPS7H2201-SP that is military grade or Automotive grade. Vin must be 1.0 - 7.0V, 6A min and must have over voltage protection
Part Number: TPS7H2201-SP Tool/software: Hello,
I wanted to ask if there is a way to disable the current limit mode while still keeping the slew rate control and short-circuit protection.
Specifically, can I set IL to ground to prevent the current…
Part Number: TPS7H2201-SP Tool/software: Hi,
Existing models for CFP devices are with straight leads. Does TI have any 3d models with bent leads (similar to gull wing packages)
Regards
Part Number: TPS7H2201-SP Tool/software: Hi team,
Please recommend the solution with in the customer request spec
1.Vin(min) <=1.7 V, Vin(max) >=3.3V
2. OVP<3.5V or adj.
3. OCP=>adj
4. current=500mA
5. Auto-retry
Part Number: TPS7H2201-SP Tool/software: Hello,
I am trying to find out how much power was applied to the device when calculating the thermal resistance junction-to-case (bottom)=0.6C/W, and junction-to-case (top)=96.1C/W for TPS7H2201-SP.
Thanks…
Part Number: TPS7H2201-SP Tool/software: Hi, I used the equation in the datasheet to adjust the ENable and OVP resistors. I still can not enable the eFuse. can you please clarify the problem ?