Part Number: TPS7H2201-SP Tool/software: I am trying to run a transient analysis simulation for TPS7H2201-SP and when I click run, it shows the log and says the file path followed by "Expected directive or device instantiation here." What does that mean…
Part Number: TPS7H2201-SP Tool/software: Hello,
I wanted to ask if there is a way to disable the current limit mode while still keeping the slew rate control and short-circuit protection.
Specifically, can I set IL to ground to prevent the current limit…
Part Number: TPS7H2201-SP Tool/software: Hi,
Is there an input capacitance (Ci) and dynamic capacitance (Cpd) available for the following part: TPS7H2201-SP? If so, can you please point me to where I can find it?
Thank you
Part Number: TPS7H2201-SP Other Parts Discussed in Thread: TPS2521 , TPS1641 Tool/software: I am currently trying to find an overvoltage protection device for my wireless receiver IC ltc4124. My overvoltage protection threshold is 5.6V. My main concern…
Part Number: TPS7H2201-SP Tool/software: Hello,
I am looking for a RAD-Hard load switch suitable for a 5V rail with a load of 3.2 Amps. The switch must feature a controlled slew rate, an enable pin, and meet radiation hardness specifications of over…
Part Number: TPS7H2201-SP Tool/software: I am looking for a part similar/identical to TPS7H2201-SP that is military grade or Automotive grade. Vin must be 1.0 - 7.0V, 6A min and must have over voltage protection
Part Number: TPS7H2201-SP Tool/software: Hello,
I'm looking for some information on the behavior of the CS output over temperature. In our temperature testing, we saw swings between +/-20% of what we expected, which is far above the +/- 10% indicated…
Part Number: TPS7H2201-SP Tool/software: Hi,
We ordered TPS7H2201HKR/EM and its QMLV part from TI. I have encountered some problems during tests of EM part. I need a solution for those unexpected results.
Firstly, I tried to use the proposed design given…
Part Number: TPS7H2201-SP Tool/software: We have an application at 1.5V Vcc switching 0.5A.
We would like to know the concerns if the tolerance of the 1.5V rail is 3% - that would drop below the recommended minimum operating voltage but above the typical…
Part Number: TPS7H2201-SP Tool/software: I need transient SPICE model for the TPS7H2201-SP. Saw from another thread that this is available, but I couldn't find it.
Thanks.
Anthony Le