Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: TPS7H2201-SP Hi expert,
Does this package have a cavity structure?
My customer is considering whether need to do a PIND(PARTICLE IMPACT NOISE DETECTION) test.
Thanks.
Part Number: TPS7H2201-SP Hi, I need the following thermal parameters for TPS7H2201-SP
Thermal Conductivity Coefficient (W/m.K)
Heat Capacity (J/kg.K)
Thank you,
Part Number: TPS7H2201-SP Hi Team,
Can you please support with dummy packages of following devices?
List of ICs used
Package
TPS7H2201-SP
CFP(HKR)16
Thanks in advance
Best Regards
Furkan Sefiloglu
Part Number: TPS7H2201-SP
Hello,
I would like some guidance as to what value of pull-down resistors to use for the CS and IL pins please.
I am not using the OVP, UVP, or the timer functions and have permanently enabled the device as shown below.
By setting…
Part Number: TPS7H2201-SP
Hi team,
Customer will change Cout, Cin from 340uF to 240uF.
Does the change of Cout only affect VOUTSR ,MAX (V/s)? Can the change of Cout affect something else?
There are no description about the change of Cin. What can the…
Part Number: TPS7H2201-SP Hello TI support,
If the current limit is removed before the IL timer expires how is the IL timer capacitor discharged?
Under this operating condition the model for the device suggests a rather long discharge time (approx. 2s…
Part Number: TPS7H2201-SP Hi Experts,
May we know if this part TPS7H2201-SP can level-shift the to -5V; that is when Vin is 0V and GND is -5V.
Still the potential difference there is +5V wrt ground.
Thank you for your assistance.
Regards, Archie A.
Part Number: TPS7H2201-SP
Can this device be configured so that the GND reference is between -3V and -5V, while Vin is 0V?
The current would flow from Vin (0V), through the device's back-to-back transistors, through the load and return through -3V (or…
Part Number: TPS7H2201-SP I want to know the power consumption of part "TPS7H2201-SP". The maximum continuous current value of "TPS7H2201-SP" is known to be 7V6/A. If you calculate the power at this time, it is 30 watt, but I don't…