Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: TPS7H2201-SP
This question is primarily in reference to this previous post .
The datasheet and the post linked above suggest that when the internal timer is used (i.e. when Pin 11 is connected to VIN) that the programmable current limit is…
Part Number: TPS7H2201-SP Other Parts Discussed in Thread: TL7700-SEP I plan to install a rad hardened undervoltage protection circuit for our NOT rad hardened OBC subsystem. It's supply voltage is 3.3V. For this application, I am eyeing a radhard eFUSE…
Part Number: TPS7H2201-SP Hello,
I have a question regarding the use of a TPS7H2201-SP. According to the datasheet, the thermal pad underneath the IC is internally connected to ground. Is it a requirement that this ground pad interface with ground on…
Part Number: TPS7H2201-SP Other Parts Discussed in Thread: TPS7H2201EVM-CVAL Hi team,
I’ve got quick questions on CERAMIC DUAL FLATPACK packages, and I’d like to confirm I understand it correct.
1. In the below figure, the lead looks floating…
Part Number: TPS7H2201-SP Hi Team,
We have received an inquiry from our customer as follows.
I have some questions about TPS7H2201-SP. (1)According to the data sheet, the OFF time of the current when turning off at the time of hard short is 61us in TYP…
Part Number: TPS7H2201-SP So you're saying that when using TPS7H2201 at low currents, I can set the current limit at a low value, RIL=1Meg for example, but the actual current limit will be 0.5A?
Part Number: TPS7H2201-SP We want to use device TPS7H2201-SP to limit the current to 2.5A. In page 9 of datasheet, it is recommended to set limit to 3.5A (IOUT + 1A). Does this mean current limit will be triggered at 3.5A? Can this be reduced to 3A cut…
Part Number: TPS7H2201-SP We are evaluating the power integrity on several rails which use the TPS7H2201 in-line.
I have checked the model and it does not really have any inductance to speak of in the Vin-Vout path.
Can you please tell me the total inductance…
Part Number: TPS7H2201-SP Hello.
I have a question about TPS7H2201-SP.
Is it possible to set the current limit on 100 mA, to watch the nominal output current in range of 80 mA?
Part Number: TPS7H2201-SP According to the SMD the OVP protection threshold has a margin between 0.52Vmin and 0.63Vmax.
To satisfy the maximum applied voltage for all downstream components after the load switch the OVP must be set to worst-case 3.6V…