Part Number: TPS7H2221-SEP Tool/software: I see that there is a parallel arrangement of this load switch for 2 in parallel from the Eval Board design.
Is it possible to have 3 in parallel? Would any issues arise if 3 of these (TPS7H2221-SEP) are in…
Part Number: TPS7H2221-SEP Can we use the TPS7H2221-SEP when the input voltage is 5.45V?
The maximum voltage of TPS7H2221-SEP is 6V.
So If we apply the derating rule, we can use this switch until +5.4V.
- Linear voltage regulator = Vin * 90% …
Part Number: TPS7H2221-SEP Tool/software: Can the ON pin be held at a voltage of 3.3V to 5V when the input is unpowered (0V)? Is it acceptable to drive the ON pin voltage to 5V when the power input (IN pin) to 3.3V?
Part Number: TPS7H2221-SEP Tool/software: We are looking at doing a monte carlo for a circuit that includes the switch and the file on the web page does not work for this in LTSpice.
Part Number: TPS7H2221-SEP Tool/software: Hi experts
I have the following questions regarding the QOD pin.
What is the peak and/or max sustained current the pin can safely discharge to GND?
What is the max amount of energy the pin can safely discharge…
Part Number: TPS7H2221-SEP Other Parts Discussed in Thread: TPS7H2221-SEP
Can more than one TPS7H2221-SEP load switch be placed in parallel to increase max current?
Part Number: TPS7H2221-SEP Hi experts
Do you have any plots or other data showing variation in Switching Characteristics (datasheet table 6.6) as a function of temperature?
tON
tR
SRON
tOFF
tFALL
Thanks for your help!
Best regards,
Jim…
Part Number: TPS7H2221-SEP
Does the input ON control pin on this part has a schmitt trigger or hysteresis built-in? Can an analog voltage signal with slow slope be used for the input ON control pin or does it have to be a digital logic signal? I could…
Part Number: SN65C1168E-SEP Other Parts Discussed in Thread: TPS7H2221-SEP Tool/software: Hello,
There are a handful of parts that i have the same question for. These parts are:
SN65C1168E-SEP
TPS7H2221-SEP
SN54SCT17-SEP
SNJ55LVDS32FK
…