Part Number: TPS7H3301-SP We are evaluating the TPS7H3301-SP VTTREF accuracy in a worst-case circuit analysis and would appreciate clarification of the ±15 mV specification.
In datasheet SLVSCJ5C, Revision C, Section 7.3.3 describes tracking half of…
Part Number: TPS7H3301-SP Hi, This is Dinesh Bala Surya from iWave global. Please find the attachment of 5962-1422801VXC circuit for verification and suggest your valuable feedback. Looking forward to your response. Regards, Dinesh Bala Surya
Part Number: TPS7H3301-SP Tool/software: Hi,
This is Dinesh from iWave Global. We are looking for the Alternate Automotive and Military Grade Part of TPS7H3301-SP with same package and same footprint. Kindly suggest us the parts, if you have. Looking…
Part Number: TPS7H3301-SP Issue with TI’s part number 5962R1422801VXC, SAT16008, reference Sandia PO 2763954. Serial Number 372 was flagged for having missing solder around the corner of the part. It seems you have had issues with TI in trying to get…
Part Number: TPS7H3301-SP Data sheet indicates that the VTTREF pin max capacitance is 2.2 uF. What is the effect of increasing this beyone the max value? Is there a stability issue or some other problem? Please provide detail... thanks!
Part Number: TPS7H3301-SP Tool/software: Hello, DS is a little confusing. What is the worst case output current or max output current capability of the part assuming a VDD of 2.5V and VLDO of 1.2V. Also, can we get a curve like that of Figure 6-13 for…
Part Number: TPS7H3301-SP Other Parts Discussed in Thread: TPS7H3302-SP Tool/software: Hello, we have an understanding that this part has a 6A inrush current with an external "band-aid" fix as the recommendation when used for DDR4 parts. Do you have a…
Part Number: TPS7H3301-SP Tool/software: Hello
Is there an input capacitance (Ci) and dynamic capacitance (Cpd) available for the part TPS7H3301?
Thank you
Part Number: TPS7H3301-SP
Tool/software:
Hello,
Im running into some stability issues with the TPS7H3301-SP and I am trying to improve the overall stability during read and write operations of DDR2.
The transients are very fast and seem to cause…