Part Number: TPS7H4001-SP The datasheet describes paralleling 4 of these devices in section 7.3.7.3. Does the below diagram still hold true for connecting 3 devices in parallel, excluding device #4?
Below is the way I've connected the three devices in…
Part Number: TPS7H4001-SP Hello E2E,
Using equation (4) on pg 27 of the datasheet, to achieve Fsw=500kHz, RT=166.2k. This is also reported by the TPS7H4001-SP Buck Converter Calculator spread-sheet.
However, the TPS7H4001-SP evaluation boards (multi…
Part Number: TPS7H4001-SP Hi Team, seeking clarification.
It is showing from bottom to top 604.5, 604.5, 604.6, 604.6, 604.6, 604.6, 604.7, 604.7, 604.7, and 604.8. Seems to be discrete and not linear. e.g at VIN from 3.75V to 5.25V , the Internal VREF…
Part Number: TPS7H4001-SP Other Parts Discussed in Thread: TPS50601A-SP ,
I am designing a board with several TPS50601A-SP converters as well as one TPS7H4001-SP.
This post for the TPS50601A-SP suggests that a 3.3V external clock source can be used to successfully…
Part Number: TPS7A4501-SP Other Parts Discussed in Thread: CDCLVP111-SP , LMK04832-SP , LMX2615-SP , TPS50601A-SP , , TPS7H1101A-SP , TPS7H3301-SP , TPS7H4001-SP Hi,
For many of TI's radiation hardened products, you also provide an /EM version intended for prototyping…
Part Number: TPS7H4001-SP We are using TPS7H4001-SP to generate 0.95V output, input is 5V. we have two CCAs, one CCA : when input changes from 4.9V to 5.1V, Vout = 0.965V. another CCA: when input changes from 4.9V to 5.1V, Vout = 0.965V to 1.025V. it looks…
Part Number: TPS7H4001-SP Other Parts Discussed in Thread: TPS50601A-SP , Hello team,
My customer is working on a design with TPS74H4001-SP and currently designing the compensation network.
Could you provide clarification on what R L is as mentioned in equation…
Part Number: TPS7H4001-SP Other Parts Discussed in Thread: TPS7H4010-SEP ,
Hi Mr./Mrs.,
After checking the reference designs of TPS7H4001-SP and TPS7H4010-SEP, the PWRGD pin is pull-high to VIN for TPS7H4001-SP while the PWRGD pin is pull-high to VOUT …
Part Number: TPS7H4001-SP If I want to operate the TPS76H4001 using the internal oscillator and a frequency different that 500 kHz, how should the SYNC1 and SYNC2 pins be set?
Table 7-1 in the data sheet indicates that SYNC1 should be floating, while…
Part Number: TPS7H4001-SP Other Parts Discussed in Thread: TPS7A4501-SP I have a question on the shutdown supply current of the TPS7H4001 – the datasheet states 2.85mA max shutdown current for VIN. Is there a specification for PVIN shutdown current…