Part Number: TPS7H4010-SEP Hello,
I built a TPS7H4010-SEP circuit based on the inverting configuration in application note SNVAA76, Radiation Tolerant Inverting Buck-Boost Converter with TPS7H4010-SEP , but the device does not seem to operate correctly…
Part Number: TPS7H4010-SEP I see that there's a VID for the TPS7H4010-SEP, V62/19623. I can't seem to determine what part class this part would be considered per EEE-INST-002 when ordered to the V62/19623 datasheet. Can you provide some insight here?…
Part Number: TPS7H4010-SEP Other Parts Discussed in Thread: TINA-TI , Hello,
I've followed this TI application note (30krad Inverting Buck Boost Converter with TPS7H4010-SEP) to get -10Vout from +12Vin using TPS7H4010-SEP. Unfortunately, my simulation…
Part Number: TPS7H4010-SEP Other Parts Discussed in Thread: TINA-TI Hello,
I am running simulations to evaluate the output voltage ripple in TINA-TI for TPS7H4010-SEP, but I have been getting much lower Vout ripple values than those listed in the datasheet…
Part Number: TPS7H4010-SEP I am looking for TPS7H4010-SEP Prompt Dose-Rate (PDR) data (both flash x-ray, FXR, and linear accelerator, LINAC). Could you please confirm whether any device-specific or family/process-level PDR data exists. NDA is acceptable…
Part Number: TPS7H4010-SEP Hello, Is there a way to change the current limitation of the TPS7h4010-SEP? The goal is to charge a battery. In the datasheet, there is only peak current limitation in HS and LS mosfet. Can this be used to try to limit the…
Part Number: TPS7H4010-SEP Tool/software: Hello,
I plan to use two TPS7H4010-SEP devices in a sequential powering configuration. The first IC will have Vout = 1.2V, and its PGood output will be connected to the EN pin of the second IC, which has Vout…
Part Number: TPS7H4010-SEP Tool/software: I am Using TPS7H4010-SEPRNP part
1. I need to help how to calculate the output current for 3.3V using 4.7uH inductor?
input voltage is 24V switching frequency set to 400 KHz
1. I also need to help how do…
Part Number: TPS7H4010-SEP Other Parts Discussed in Thread: LM73606
Tool/software:
Hi TI,
I've been working on an inverting buck-boost converter utilising the TPS7H4010-SEP based on the application note SNVAA76 - Radiation Tolerant Inverting Buck…
Part Number: TPS7H4010-SEP I need to generate a negative voltage (e.g. application note snvaa76.pdf). Input voltages available are 3.3 and 6.5. Output voltage necessary is anything between -5 and -3V (less than 75mA). I need better than 75kRad TID spec…