Part Number: TPS7H5005-SEP Tool/software: Hello,
I am trying to use the TPS7H5005 as a controller for a flyback circuit, and would like the ability to periodically turn off the controller. When I try to either lower EN to 0 or raise FAULT to 3.3, the…
Part Number: TPS7H5005-SEP Other Parts Discussed in Thread: TPS7H5001-SP , TPS7H6013-SP , TPS7H5006EVM Tool/software: Hello. I'm working on a 12 V to 1 V buck converter which will use a TPS7H5005-SEP and TPS7H6013-SP. I'm trying to use DCR current sensing…
Part Number: TPS7H5005-SEP Tool/software: I would like to get some details regarding the IC "TPS7H5005-SEP". Since the product details mentions that this IC can be used for Boost converter design as in the attached image, I would like to get the schematic…
Part Number: TPS7H5005-SEP Tool/software: Dear team,
As per the datasheet TPS7H5005-SEP can be used for multiple typologies but application schematic is not available for single switch forward converter so kindly share any application schematic or elaborate…
Part Number: TPS7H5005-SEP Other Parts Discussed in Thread: PMP23193 , TPS7H5001-SP , Tool/software: I would like to use the TPS7H5005 / 5001 in a push-pull application, similar to the reference design in the datasheet. Whenever I try to simulate the…
Part Number: TPS7H5005-SEP Other Parts Discussed in Thread: PSPICE-FOR-TI Hello, I have been trying to execute a simulation for TPS7H5005-SEP, however I am consistently getting an error regarding imported models with the simulation that was given through…
Part Number: TPS7H5005-SEP Hello,
I just wanted to follow up with the updated TPS7H5005-SEP PSpice model added to the device page. After attempting to run the PSpice file, I was unable to successfully complete the simulation. I do have the auto converge…
Part Number: TPS7H5005-SEP Is there recommended topology on the secondary for synchronous operation? I plan to use GaN drivers at secondary output and there should probably be a power source to drive the secondary GaN FETs. Can you please point me in…
Part Number: TPS7H5005-SEP Other Parts Discussed in Thread: TPS7H5001-SP , Hello,
Is there a reference design using the TPS7H5005 part in a non-isolated synchronous buck design? I have something working 90% but I need some help with some of the compensation…
Part Number: TPS7H5005-SEP Other Parts Discussed in Thread: UC1708-SP I am trying to build a push pull isolated DC/DC converter. Vin 26-34V, Vout 28V, Iout 10A. I am not opposed to using two converters to share the load using the Sync pin. My use case…