Part Number: TPS7H6003-SP Hey guys,
Would there be any issue using the TPS7H6003-SP to drive both the hide and low primary-side switches in a flyback topology with an external bootstrap diode and capacitor?
My sneaking suspicious is that due to…
Part Number: TPS7H6003-SP Other Parts Discussed in Thread: TPS7H5001-SP Hello, I am trying to simulate TPS7H6003-SP with TPS7H5001-SP. In the simulation files on your website the model is written in the command window for each separetly. what should I…
Part Number: TPS7H6003-SP Other Parts Discussed in Thread: TPS7H5001-SP Hi, We would like to use TPS7H6003-SP with TPS7H5001-SP PWM controller to drive a Push Pull converter with SR. we have the schemtic below but without SR, can you suggest how the Schemtic…
Part Number: TPS7H6003-SP Other Parts Discussed in Thread: TPS7H5001-SP , , TPS7H5020-SP Tool/software: Hello
I have a system that is doing a 5V to 0.8V using the TPS7H5001-SP and TP7H6003-SP as a buck controller.
What I missed, is that the TPS7H6003…
Part Number: TPS7H6003-SP Tool/software: Dear Team,
My customer is looking at the TPS7H6003HBX and the TPS7H6023HBX, and checking the package information of the datasheet. Since there is not information of the Metal mask opening dimensions, they would…
Part Number: TPS7H6003-SP Tool/software: Hello,
The datasheet for the TPS7H6003-SP doesn't have listed a maximum/minimum switching frequency range for this device. We are planning to use this device with the Independent input mode enabled.
I understand…
Part Number: TPS7H5001-SP Other Parts Discussed in Thread: TPS7H6003-SP
Tool/software: Simplis
Hi,
I'm designing a Full Bridge DCDC Converter with 24-38V input and 30V/20A output using TPS7H5001-SP and TPS7H6003-SP. I am referring to one of the…
Part Number: TPS7H6003-SP I'm looking to build a syncronus dcdc boost converter to go from 12V to 200V based on the topology below. The PWM signals will be generated by a microcontroller running a control loop. This is needed so the output voltage can…
Part Number: TPS7H6003-SP Other Parts Discussed in Thread: TPS7H5003-SP I'm interested in using the TPS7H600X-SP gate drives for synchronous buck and boost applications, paired with the TPS7H5003-SP PWM controller.
1. Does Texas Instruments have any…
Part Number: TPS7H6003-SP In the description of the Input Interlock Protection (8.3.7) are we to assume that using a resistor between DLH and ground, of some value between 100k and 220k, somehow sets the universal deadtime for the device when using the…