Other Parts Discussed in Thread: TPS81256 , TPS53355 Hello, The customer would like to use TPS81256 for VDD of TPS53355.
(1) Start Up time In the TPS81256 datasheet P.5, the start up time from active EN to start switching is 70us. Please see the attached file…
Other Parts Discussed in Thread: TPS81256 , TPS61251 Dear Sir
My customer is use TPS81256 in 3.3Vin and Vout 5V application in SSD product.
Due to have super cap function, my customer paraell 1.6mF capacitor in output.
then sometime will case 3.3Vin voltage…
Part Number: TPS81256EVM-121 Other Parts Discussed in Thread: TPS81256 , BQ24075 , TPS61027 , TPS61022 Hello,
The input of the TPS81256-EVM is provided by a BQ24070X-EVM. When powered from either the battery or USB, the output of the TPS81256 is 5.0V as expected…
Hi Shmuel,
If you cannot work with WCSP package, you can consider using TPS81256, which integrate input/output capacitor, inductor, IC. The device package is 2.9mm x 2.6mm with 1mm pitch.
Other Parts Discussed in Thread: TPS81256 , TPS61240 I am using the TPS81256 Eval Board. I am powering it with 3.3V external power supply. The output has a resistor (25, 50, or 150Ohm). I do not get 5V on the output. With the 50Ohm resistor, I get ~2.8V…
Other Parts Discussed in Thread: TPS81256 , TPS81256EVM-121 , TPS60400 Hi,
The spec sheet for the TPS81256 states that in most applications an external input capacitor is not needed (since there is already a built-in one). However, the TINATI transient model…
Part Number: LM25118 Other Parts Discussed in Thread: TPS81256 , , TPS61022 , TPS552882 When using as a booster for input 3V to 4V and output 5V、It operated by applying 5V boosted from TPS81256 to 1pin (Vin), 17pin (VCCX), and 10pin (VOUT).
Is it suitable…
Hi Shahriyar,
Currently the power module's team is invested in step down modules. The only boost power module that comes to mind is the TPS81256. For a 3V input voltage and 5V output voltage, the maximum output current using the TPS81256 is roughly ~560mA…
I am replying since Jasper is out. I found one device(TPS81256) which integrated inductors in MicroSiP package, but it seems it doesn't support 10Vout.
Regards,
EL