Part Number: TPS82084 Hi team,
Could you let us know the AU deposit thickness at the lead part?
If you can not, could you show us the material content of the lead?
Best regards,
Yuta Ishii
Part Number: TPS82084 Hello,
My customer would like to know the recommended pull-up resisstor values for PG and EN of the TPS82084.
When using 3.3V pull-up voltage, what is the recommended pull-up resistor value for PG and EN? How should the customer…
Part Number: TPS82084TPS82084 using as below: Vsys is from Single Battery voltage.
When the input voltage is lower than output voltage required, the TPS82084 Vout will lock at 2.2V.
We haven't find any description about this.
There're only 2 descriptions…
Part Number: TPS82084 Other Parts Discussed in Thread: LM3880 I am using two of the TPS82084's to power two different rails on a part. The rails are 1.8V and 0.9V. I have a requirement where I need to power up the 0.9V first and then the 1.8V. However…
Part Number: TPS82084 Other Parts Discussed in Thread: TPS82140 I'm considering using the TPS82084 to supply a power rail that has a minimum ramp time of 0.2 ms. The TPS82084 datasheet lists a typical ramp time of 0.8 ms, but gives no minimum value…
Part Number: TPS82084 Hi,
I have used the TPS82084SILT for 5V to 3.3V conversion with 499k as PG pull-up, R2=150k,R1=465K.
Input voltages measured are: EN,VIN are 5V
But output is zero.
The inductor above the IC is measuring 4.35V on one side(near to…
Part Number: TPS82084 Hello.
In the data sheet, there is a paragraph about output capacitor, which states "no more than 150uF"(page 11). Is that includes all the load capacitors? for example, if my load is a FPGA which requires a 330 uF capacitor- can…
Part Number: TPSM82822 Other Parts Discussed in Thread: TPS82084 , ADC12DL2500 Tool/software: Hi Team,
We have ADC (P/N: ADC12DL2500) in our design, For ADC VLVDS (5V input, 1.9V output 0.5A Load current) input we have old part (P/N: TPS82084) RθJA: 64.6…
Part Number: TPS82084 Other Parts Discussed in Thread: TPS82130 , TPS82140 , TPS82150 , TPS82085 Hello,
I would like to use TPS82084 and TPS82130 ICs in one of my new designs as these are the newly arrived. I could see "Manufacturing delays have been reported…