Part Number: TPS82085 Hi,
The datasheet says "This pin has an internal pull-down resistor of typically 400 kΩ when the device is disabled." I think it means, when I pull the EN down to below 0.4V, the pull-down will take effect, right? Then why use…
Part Number: TPS82085 Hi Team,
Can you please explain the difference between the terms thermal resistance VS characterization parameter?
Would it be effective to add heatsink at the top of this package?
Thanks.
Part Number: TPS82085 Other Parts Discussed in Thread: TPSM82823 As per the REACH 17 Jan 2023 update, melamine substance should not be present more than 0.1% in homogeneous material. We are using your part TPS82085SILR in our product, which contains 3…
Part Number: TPS82085
Please explain this logic.When pulling up or floating on PG,why is PG compared to Vfb? If pulled up, Vfb cannot be larger than PG, and if floating, it is meaningless!
Part Number: TPS82085 Hi,
Is this part susceptible to latchup?
Is the part of bipolar technology?
are you aware of any radiation data (total dose, SEE)?
Part Number: TPS82085 Hi,
I have received a lot of TPS82085SILR from a broker. According to packet stickers the date code informations are : 20+
Do you have the eplanation of the way to interpret these date code informations ?
Thank a lot for your…
Hi,
I received part number: TPS82085SILR date code 2229. DC to DC converter. Part marking GE.
I would like to know the country of origin for this type of part.
Thanks for your time.
Part Number: TPS82085 Hi,
Customer observed there is slight discolorations on the inductor surfaces for this SIP module sample part (yellow discoloration portion pointed out in red arrows below):
This part contains fairly new DC (2239) and so customer…