Part Number: TPS82130 Other Parts Discussed in Thread: TPSM82903 Hi team,
Do we have smaller module compared with TPS82130? Input is 12V, Iout <3A.
Nison
Part Number: TPS82130 Dear Support,
I have one board out of a lot of 6 that doesn't work. because this package is very small, so it is very hard to check the soldering. I checked Vout to Vin( I saw there is a diode), and also found a diode between Vout…
Part Number: TPS82130
Hi,
Good Day.
What is the expected true power (delivered) of the device with 1V/1.8A?
What is the power dissipation (wasted) with respect to ambient temperature?
Please advise. Thank you very much.
Best Regards,
Ray Vincent
Part Number: TPS82130 Other Parts Discussed in Thread: TPSM82903 , TPSM82913 Hello,
What is the absolute max junction temperature of TPS82130? The datasheet table of Absolute Max Ratings shows 125C for Module operating Temperature. What temperature is…
Part Number: TPS82130 Other Parts Discussed in Thread: TIDA-01457 Hi Expert.
My customer is willing to use TPS82130 in their new project for negative output. I promote TIDA-01457 and I have a small question. Will our design have any impact on the system…
Hi Nancy,
My customer wants to use the LM66100 for the output stage of the TPS82130, the VOUT they use is 4.2V. Isn't it recommended to use the LM66100 for the output stage?
Thanks,
JH
Part Number: TPS82130 Other Parts Discussed in Thread: TPS543320 Hi team,
This is Jayden, I have question about the OCP. The Test conditions is Vin=12V and Vout=3.3V. The waveform below is Vout.
The Vout drops when Iout=3.5A (As I calculate, ΔIL=1.196A…