Part Number: TPS82150 Hi
I posted following URL, but I the post may not have arrived, so I will repost it.
e2e.ti.com/.../tps82150-tps82150-start-up-time
I want to ask about TPS82150's start up time.
I simulated TPS82150's start up sequence using…
Part Number: TPS82150 Dear team ,
In my board design , there are two power supplier 5V and 3.3V . They are not exist at the same time . And 3.3V is the main power for whole board.
So i use TPS82150 for power conversion : 5V To 3.3V .
But there is…
Other Parts Discussed in Thread: TPS62913 , TPS62912 Hi team,
We are using TPS and TPSM integrated inductor modules on the FPGA side(an RF product).some rails are taking low current, its switching frequency is low(below1Mhz). Do we need to add a second…
Part Number: TPS82150 To whom may it concern,
I want to know timing information about TPS82150.
I use Vin = 9V, Vout = 3.3V.
Vout's start-up timing does not matter, but I hope Vout's blocking timing is fast.
So, How fast Vout is blocked after…
Part Number: TPS82150 Section 7.3.2 of the datasheet describes the minimum input V for LDO/100% duty cycle mode but there is no indication of what condition(s) cause the IC to enter this mode. Is it possible to force this mode?
My design is 12V in, 3…
Part Number: TPS82150 Other Parts Discussed in Thread: TPS62160 Hi team,
I wonder if the customer can replace TPS62160 with TPS82150. I want to suggest TPS82150 as a small and simple design alternative to TPS62160. Is it valid in term of the performance…
Part Number: TPS82150 Other Parts Discussed in Thread: LMZ21701 , TPSM84203 , Team,
Some comparable modules (like TPSM84203 and LMZ21701) do include conducted/emitted EMI tested curve in the datasheet. Do we plan to include it for TPS82150?
More generally…
Part Number: TPS82150 I think this is ok because datasheet says up to 7V absolute max. without any parametric dependence on VIN, and section 7.4.4 of the datasheet says that PG goes high impedance withe VIN
Part Number: TPS82150 Other Parts Discussed in Thread: TIDA-01405 Tool/software: WEBENCH® Design Tools Hi,
as defined in TIDA-01405 design, TPS82150 can be used as negative voltage source.
However the simulation model (both for TINA and PSPICE) does not…
Part Number: TPS82150 Hi Team, we would like to confirm for the max height of the substrate with pads and mask.
Thank you very much.
Regards,
Mark Felipe