Hi Robert,
Thanks for replying
1. So the idea is by turning on/off/open 3.3V GPIO to change the voltage level on VADJ pin and adjust the VOUT of LMZ31503. Am I correct?
if so, how can I calculate the resistor value with TPS84320?
3. I work in Hong …
Other Parts Discussed in Thread: TPS84320 I have some questions about TPS84320 ,i can not sure.
For the simple use the chip of TPS84320 , according to the datasheet about TPS84320, i can float these pins as followed :"INH/UVLO","SS/TR","PWRGD" ,can i …
Other Parts Discussed in Thread: TPS84320 , LMZ14203H , LMZ12003 Sorry if this is in the wrong forum...
Can the integrated power modules be hooked up to proved a negative 5V like the LTM8025 (see page 16)
http://cds.linear.com/docs/Datasheet/8025fa.pd…
Other Parts Discussed in Thread: TPS84320 The schematics of PMP8571 shows that Rset for 3.3V and 1.5V are the same value of 1.74K while the RRT as 324K for TPS84320. Assuming that there is a typo somewhere but no of the value fit the datasheet. According…
Hello Tsukui-san,
With FPGA's their actual power needs vary depending on the clock speed and other variables.
Therefore many times TI does not have a design for a specific FPGA.
One good way to build a design is to use Webench FPGA Architect.
XCZU4CG…
Other Parts Discussed in Thread: TPS84620 Hello team,
Can we use any of our integrated-inductor buck converters (TPS84620, for example) in inverting buck-boost configuration? I am referring to the slva257a app note which shows that we basically need to…