Part Number: TPS84410 Other Parts Discussed in Thread: LMZ30604 Hello TI experts,
Are TPS84410 and LMZ30604 the same?
there are no differences between these 2 parts, including package, pin map, block diagram, even electric characteristics.
Please confirm…
Part Number: TPS84410 Other Parts Discussed in Thread: LMZ30604 , TPSM82864A Please let me know about internal Inductance value(μH) of TPS84410 (or LMZ30604).
In the past I post below E2E thread, but I lost Email history and could not contact now.
…
Part Number: TPS84410 Other Parts Discussed in Thread: TPSM82480 , TPSM82810 I tried creating a footprint for this part but the datasheet is obviously wrong. It shows the distance between pad 1 and pad 2 is 1.45mm but when I do that the pads overlap. Please…
Part Number: TPS84410 Hi team,
My customer is using TPS84410 in their design, and the schematic is the typical application in the datasheet. The input voltage is 5V, output voltage is set to 3.3V. The problem is the real output voltage is 2.93V which…
Part Number: TPS84410 PLs find the attached schematics
I need to generate a 0.95V core voltage output with 3% accuracy.
I would like to have an isolation feature to test. is the arrangement ok?? Is the placement of capacitors ok??
pls suggest
Part Number: TPS84410 Dear Team, Please provide the FIT Value of following components for Reliability analysis. Test temperature, Confidence level, Activation energy values also required. DS90C032TM/NOPB Tried TI website also but for these parts data is…
Hello,
I am getting an occasional drop out on my regulator. I believe that part of the issue is I am getting noise coupled into the feedback path (which is located on the bottom layer of my design). I was able to minimize this by adding a faraday shield…
Other Parts Discussed in Thread: TPS84410 Hello I am thinking of using the TPS84410 in the following scenario.
Vin = 3.3V +/- 5%
Vout = 1.8V
load= up to 4A
The 3.3V is coming from a switched supply on another PCB and it will be noisy. My concern is the…
Other Parts Discussed in Thread: TPS84410 , SN65HVD232Q Hi,
Can you provide the TID(Total Ionisation data) for the Below mentioned IC..?
1.TPS84410
2.SN65HVD232Q