Hi Vishal,
As explained in the D/S, the TPS62140 enters power save mode for light loads and here it reduces the switching frequency.
Since you are also using the TPS84620 module, you might like to use the TPS82140 module version of the TPS62140…
Part Number: LMZ31503 Other Parts Discussed in Thread: LMZ31506 , I have question about RRT: switching frequency setting resister for LMZ31503 and LMZ31506, please see below.
①The below thread is described RRT accuracy is ±20%, but high fsw condition…
Other Parts Discussed in Thread: TPS84620 Hello team,
Can we use any of our integrated-inductor buck converters (TPS84620, for example) in inverting buck-boost configuration? I am referring to the slva257a app note which shows that we basically need…
Hi Rafael,
Currently we do not have any model for TPS84620. Can you use the TPS84621 model for your testing as it is very much similar to TPS84620 from a working point of view.
Best regards,
Nikhil
Other Parts Discussed in Thread: TPS84620 There is this post “TPS84620 used as LED driver” Although I do not need to drive LED’s the question is essentially the same.
The target devices I have picked are the: TPN78000/78020/78060 These are all voltage…
Just a thought. Please verify the part number of the device with the incorrect output voltage. TPS84620 has an internal 0.8V reference, while the TPS84621 has an internal reference of 0.6V. This would explain why the output voltage is 2.5V. Both parts…
Other Parts Discussed in Thread: TLC59108 , TPS84620 , TLC59116 Hello,
Thank you in advance for any help offered. I am working with a software engineer who will help this end, but am currently am stuck for solutions.
Our circuit consists of 3x TLC59108…
Other Parts Discussed in Thread: TPS84250 Hi,
I'm interesting in the next topic - today there are parts in the the LMZ3 and TPS84k family which have different part numbers but they are " EXACT EQUIVALENT in functionality and parametrics to the compared…