Part Number: TPS84A20 Hi,
TPS84A20 has two types of ground, PGND and AGND. According to the datasheet, PGND is the return current path for the power stage of the device and AGND is the zero volt reference for the analog control circuit. In the Layout…
Other Parts Discussed in Thread: TPS84A20 Hello, I'm Alber as a FAE in Arrow Korea. My customer will use the TPS84A20 to supply FPGA and other digital Core voltage. V_in is 5.6V and V_out is 3.3 or 1.0V. They are considering the input voltage quality. …
Other Parts Discussed in Thread: TPS84A20 I'm looking for information on the nominal value and tolerance of the inductor inside this part. Also does it have any current ratings? 90% nominal at X Amps, 80% nominal at Y Amps.
Other Parts Discussed in Thread: TPS84A20 , LMZ31710 Hello Team,
My customer uses the TPS84A20 on a board and they did not connect AGND and PGND of TPS84A20. It was communicated at the time that for the TPS84A20 it is connected internally. Therefore, we…
Other Parts Discussed in Thread: TPS84A20 , LMZ31710 Hi,
Can someone point out the difference between TPS84A20 and LMZ31710? I saw that LMZ is preferred but I could not figure out the reason for that.
Thanks!
Hi Khoi,
What are your input and output voltages? What is your output current?
TPS84A20 is a direct replacement for LMZ31710, but TPS84A20 seems to be out of stock as well !
You may want to look at PTD08A210W, PTD08D210W, PTD08A10W, PTH08T241W and PTH08T240W…
Other Parts Discussed in Thread: PMP , TPS84620 Hello,
what's the difference between the two? I read the datasheet but they seem equivalent.
Thanks
Best Regatds
Giacomo
Part Number: LMZ31710 Other Parts Discussed in Thread: TPS84A20 Hi there,
Part shortage issue, LMZ31710RVQR part is out of stock currently and I need to get an estimate time for availability. or is there any drop in compatible alternatives.
Thanks,
Azar
Other Parts Discussed in Thread: TPS84A20 , LMZ31710 7178.TPS84A20RVQR package.pdf
Hi
Let me know about the No.1~No.11 of attachment file.
Product:TPS84A20(LMZ31710)
①3.29mm?
②
③0.95mm?
④1.4mm?
⑤1.7mm?
⑥
⑦
⑧3.28mm
⑨
⑩0.525mm
⑪4.05mm
I already checked below…
Other Parts Discussed in Thread: TPS84A20 I have an application which looks perfect for the TPS84A20, except the output voltage required is +6V. From the equation, it looks like a value of 159 ohms would set it to 6V. With the higher output voltage, the…